<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: NXP Support in Android Lollipop 5.0.0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/NXP-Support-in-Android-Lollipop-5-0-0/m-p/588460#M88936</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SergioSolis, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Thanks for the reply. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I am able to add the NFC driver and it is working with the PN7120 NFC&lt;/P&gt;&lt;P&gt;Chip connected to our embedded board. The node is being detected too. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I was expecting that the Android Porting Guidelines document from NXP&lt;/P&gt;&lt;P&gt;was sufficient to make the NFC working. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; So from your reply I can understand that the NXP supporting APIs are&lt;/P&gt;&lt;P&gt;missing in my AOSP code (Correct me if I am wrong) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; The Android source Lollipop source code downloaded by our team has&lt;/P&gt;&lt;P&gt;removed the ./repo/ folder completely and ported the source code so that&lt;/P&gt;&lt;P&gt;it boots for our custom board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; So will the NFC API's will be added to the Android framework with "make&lt;/P&gt;&lt;P&gt;update-api" command ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Or do I need to go for a repo sync of the whole Android Lollipop git&lt;/P&gt;&lt;P&gt;source code for making NFC possible? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Awaiting your valuable suggestions. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anjali &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On 10.08.2016 11:43, SergioSolis wrote: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE level="1"&gt;&lt;P&gt;NXP COMMUNITY &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP SUPPORT IN ANDROID LOLLIPOP 5.0.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from SergioSolis  in &lt;U&gt;i.MX Community&lt;/U&gt; - View the full discussion &lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Aug 2016 05:37:21 GMT</pubDate>
    <dc:creator>anjalikkrishna</dc:creator>
    <dc:date>2016-08-11T05:37:21Z</dc:date>
    <item>
      <title>NXP Support in Android Lollipop 5.0.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-Support-in-Android-Lollipop-5-0-0/m-p/588458#M88934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working on NFC in Android Lollipop 5.0.0. My team has successfully made the NFC working in kernel level. We had used PN71x0 Linux Software Stack Integration Guidelines document from NXP for this. I followed the NFC Android Porting Guidelines from the link &lt;A href="https://github.com/NXPNFCLinux/nxpnfc_android_lollipop/blob/master/AN11690%20-%20NXPNCI%20Android%20Porting%20Guidelines.pdf" title="https://github.com/NXPNFCLinux/nxpnfc_android_lollipop/blob/master/AN11690%20-%20NXPNCI%20Android%20Porting%20Guidelines.pdf"&gt;nxpnfc_android_lollipop/AN11690 - NXPNCI Android Porting Guidelines.pdf at master · NXPNFCLinux/nxpnfc_android_lollipop …&lt;/A&gt;&amp;nbsp; to make the NFC working in Android level. But the NFC option is missing under Settings-&amp;gt; more. I have added nfc under required_hardware.xml file and also other changes as per the above document.&amp;nbsp; Is there anyway to enable the NFC option in UI ? .&amp;nbsp; I am not able to get any NFC related logs too except one saying " Could not retrieve NFC service". &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I request for support to make the NFC working in Android lollipop. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 05:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-Support-in-Android-Lollipop-5-0-0/m-p/588458#M88934</guid>
      <dc:creator>anjalikkrishna</dc:creator>
      <dc:date>2016-08-10T05:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Support in Android Lollipop 5.0.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-Support-in-Android-Lollipop-5-0-0/m-p/588459#M88935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anjalik&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to rebuild android so the api changes take effect with the following command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;make update-api&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is after you download the local manifest and run the installation scripts and patches.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were you able to add the NFC driver?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 15:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-Support-in-Android-Lollipop-5-0-0/m-p/588459#M88935</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2016-08-10T15:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Support in Android Lollipop 5.0.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/NXP-Support-in-Android-Lollipop-5-0-0/m-p/588460#M88936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SergioSolis, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Thanks for the reply. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I am able to add the NFC driver and it is working with the PN7120 NFC&lt;/P&gt;&lt;P&gt;Chip connected to our embedded board. The node is being detected too. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I was expecting that the Android Porting Guidelines document from NXP&lt;/P&gt;&lt;P&gt;was sufficient to make the NFC working. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; So from your reply I can understand that the NXP supporting APIs are&lt;/P&gt;&lt;P&gt;missing in my AOSP code (Correct me if I am wrong) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; The Android source Lollipop source code downloaded by our team has&lt;/P&gt;&lt;P&gt;removed the ./repo/ folder completely and ported the source code so that&lt;/P&gt;&lt;P&gt;it boots for our custom board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; So will the NFC API's will be added to the Android framework with "make&lt;/P&gt;&lt;P&gt;update-api" command ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Or do I need to go for a repo sync of the whole Android Lollipop git&lt;/P&gt;&lt;P&gt;source code for making NFC possible? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Awaiting your valuable suggestions. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anjali &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On 10.08.2016 11:43, SergioSolis wrote: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE level="1"&gt;&lt;P&gt;NXP COMMUNITY &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP SUPPORT IN ANDROID LOLLIPOP 5.0.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from SergioSolis  in &lt;U&gt;i.MX Community&lt;/U&gt; - View the full discussion &lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 05:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/NXP-Support-in-Android-Lollipop-5-0-0/m-p/588460#M88936</guid>
      <dc:creator>anjalikkrishna</dc:creator>
      <dc:date>2016-08-11T05:37:21Z</dc:date>
    </item>
  </channel>
</rss>