<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX53 expansion header data line control</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186743#M8893</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey guys, I am interfacing several LCDs to the i.mx53 quick start board via a custom daughter board utilizing the expansion header.&amp;nbsp; I can get 2 of the 3 LCDs to work perfect, however the last one has some color skewing.&amp;nbsp; I believe the problem stems from the fact that the display data lines on the LCD side need to be bit shifted.&lt;/P&gt;&lt;P&gt;The expansion port connector pins 108-62 correspond to Display Data 23 - Display Data 00, 8 bits each RGB.&amp;nbsp; Both of the LCDs that are working properly are 24 bit color.&amp;nbsp; The problem LCD is 18 bit color as the RGB mapping does not seem correct.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Rather than cut and jumper those 18 tiny connections, does anyone know if this can be fixed in software--either at the command line level or even with a special build of the kernel that modifies the mapping either between the ipu and the pads or between the framebuffer and the ipu?&amp;nbsp; Any help would be greatly appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Joey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Sep 2012 17:27:22 GMT</pubDate>
    <dc:creator>Joey</dc:creator>
    <dc:date>2012-09-06T17:27:22Z</dc:date>
    <item>
      <title>i.MX53 expansion header data line control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186743#M8893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey guys, I am interfacing several LCDs to the i.mx53 quick start board via a custom daughter board utilizing the expansion header.&amp;nbsp; I can get 2 of the 3 LCDs to work perfect, however the last one has some color skewing.&amp;nbsp; I believe the problem stems from the fact that the display data lines on the LCD side need to be bit shifted.&lt;/P&gt;&lt;P&gt;The expansion port connector pins 108-62 correspond to Display Data 23 - Display Data 00, 8 bits each RGB.&amp;nbsp; Both of the LCDs that are working properly are 24 bit color.&amp;nbsp; The problem LCD is 18 bit color as the RGB mapping does not seem correct.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Rather than cut and jumper those 18 tiny connections, does anyone know if this can be fixed in software--either at the command line level or even with a special build of the kernel that modifies the mapping either between the ipu and the pads or between the framebuffer and the ipu?&amp;nbsp; Any help would be greatly appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Joey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2012 17:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186743#M8893</guid>
      <dc:creator>Joey</dc:creator>
      <dc:date>2012-09-06T17:27:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 expansion header data line control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186744#M8894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Joey&lt;/P&gt;&lt;P&gt;We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the &lt;/P&gt;&lt;P&gt;issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 08:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186744#M8894</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-14T08:52:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 expansion header data line control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186745#M8895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Joey&lt;/P&gt;&lt;P&gt;We have not got your response yet and will close the diacussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 05:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186745#M8895</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-24T05:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX53 expansion header data line control</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186746#M8896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 03:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX53-expansion-header-data-line-control/m-p/186746#M8896</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-03-03T03:22:29Z</dc:date>
    </item>
  </channel>
</rss>