<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6 git sync not working properly in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-git-sync-not-working-properly/m-p/587802#M88887</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Santhosha, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried downloading the tzdata file and the FTP works. I also tested the git from Freescale and had no problems. I would recommend making sure that you have internet access from your host. Sometimes proxys may cause errors with git. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Martin Mauer is suggesting, try reaching the Freescale git or the tzdata file from outside bitbake to test your connection and if you are using a proxy or if you are behind a firewall check your settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jul 2016 19:22:06 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-07-19T19:22:06Z</dc:date>
    <item>
      <title>imx6 git sync not working properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-git-sync-not-working-properly/m-p/587800#M88885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;imx6 git sync not working properly,&amp;nbsp; why is it so?&amp;nbsp; please guide...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ARNING: Failed to fetch URL &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=ftp%3A%2F%2Fftp.iana.org%2Ftz%2Freleases%2Ftzdata2015b.tar.gz%3Bname%3Dtzdata" rel="nofollow" target="_blank"&gt;ftp://ftp.iana.org/tz/releases/tzdata2015b.tar.gz;name=tzdata&lt;/A&gt;&lt;SPAN&gt;, attempting MIRRORS if available&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;ERROR: Fetcher failure: Fetch command failed with exit code 128, output:&lt;/P&gt;&lt;P&gt;fatal: unable to connect to git.freescale.com:&lt;/P&gt;&lt;P&gt;git.freescale.com[0: 192.88.156.202]: errno=Connection refused&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Function failed: Fetcher failure for URL: 'git://git.freescale.com/imx/linux-2.6-imx.git;protocol=git;branch=imx_3.14.38_6ul_ga'. Unable to fetch URL from any source.&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/santhosh/fsl-release-bsp/build-wayland/tmp/work/imx6sxsabresd-poky-linux-gnueabi/linux-imx/3.14.38-r0/temp/log.do_fetch.5063&lt;/P&gt;&lt;P&gt;ERROR: Task 73 (/home/santhosh/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_3.14.38.bb, do_fetch) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 1701 tasks of which 1075 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /home/santhosh/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_3.14.38.bb, do_fetch&lt;/P&gt;&lt;P&gt;Summary: The&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 15:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-git-sync-not-working-properly/m-p/587800#M88885</guid>
      <dc:creator>santhosha</dc:creator>
      <dc:date>2016-07-19T15:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 git sync not working properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-git-sync-not-working-properly/m-p/587801#M88886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you tried if you can reach the address via FTP without the script?&lt;/P&gt;&lt;P&gt;Are you perhaps behind a firewall and need a proxy?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 17:35:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-git-sync-not-working-properly/m-p/587801#M88886</guid>
      <dc:creator>martin_maurer</dc:creator>
      <dc:date>2016-07-19T17:35:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 git sync not working properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-git-sync-not-working-properly/m-p/587802#M88887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Santhosha, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried downloading the tzdata file and the FTP works. I also tested the git from Freescale and had no problems. I would recommend making sure that you have internet access from your host. Sometimes proxys may cause errors with git. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As Martin Mauer is suggesting, try reaching the Freescale git or the tzdata file from outside bitbake to test your connection and if you are using a proxy or if you are behind a firewall check your settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 19:22:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-git-sync-not-working-properly/m-p/587802#M88887</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-07-19T19:22:06Z</dc:date>
    </item>
  </channel>
</rss>