<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mfg-tool stuck on Sending partition shell</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-stuck-on-Sending-partition-shell/m-p/587307#M88828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adriaan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if baord stucks with no debug this may be due to memory errors.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Also one can try to execute these commands from linux, as mfg tools just runs&lt;/P&gt;&lt;P&gt;small linux image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jun 2016 08:02:55 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-29T08:02:55Z</dc:date>
    <item>
      <title>mfg-tool stuck on Sending partition shell</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-stuck-on-Sending-partition-shell/m-p/587306#M88827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;We are using the mfg-tool to setup a custom board based on the iMX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have built updated versions of the mfg U-Boot, kernel, root file system, and device tree for our HW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mfg-tool detects the board when powered up, sends U-Boot, kernel, rfs and dtb and successfully jumps to U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot successfully starts the kernel and the mass storage device comes up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the mfg-tool tries to execute the push send for mksdcard_new.sh.tar (Sending partition shell) step but gets stuck with no debug on the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any recommendations, ideas, debug I need to provide?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Adriaan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 05:47:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-stuck-on-Sending-partition-shell/m-p/587306#M88827</guid>
      <dc:creator>adriaanswanepoe</dc:creator>
      <dc:date>2016-06-29T05:47:27Z</dc:date>
    </item>
    <item>
      <title>Re: mfg-tool stuck on Sending partition shell</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-stuck-on-Sending-partition-shell/m-p/587307#M88828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adriaan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if baord stucks with no debug this may be due to memory errors.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Also one can try to execute these commands from linux, as mfg tools just runs&lt;/P&gt;&lt;P&gt;small linux image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 08:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfg-tool-stuck-on-Sending-partition-shell/m-p/587307#M88828</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-29T08:02:55Z</dc:date>
    </item>
  </channel>
</rss>