<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI Mux - non gpio cs in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587196#M88809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi matthew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according documentation and probe function in linux/drivers/spi/spi-imx.c&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_3.14.28_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/spi/spi-imx.c?h=imx_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/spi/spi-imx.c?h=imx_3.14.28_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;CODE&gt;seems implemented only option with "cs-gpios".&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Aug 2016 01:01:00 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-08-10T01:01:00Z</dc:date>
    <item>
      <title>SPI Mux - non gpio cs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587195#M88808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Im trying to set up a device tree for some custom hardware and had a mux question regarding SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ive looked at the imx6qdl-nitrogen6_max.dtsi as part of the boundary 3.14 linux release. The spi chipselects in the nitrogen and sabre boards are all tied to GPIO's however our spi CS isnt done using gpio. For example Spi 1's ss0 is on pin disp0_data23. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current device tree sets spi CS up as:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl,spi-num-chiselects = &amp;lt;1&amp;gt;&amp;nbsp;&amp;nbsp; (this should be ok for ours as well)&lt;/P&gt;&lt;P&gt;cs-gpios = GP_ECSPI1_NOR_CS&lt;/P&gt;&lt;P&gt;where&lt;/P&gt;&lt;P&gt;GP_ECSPI1_NOR_CS is a #define pointing to a gpio bank and pin. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If were using the disp0 line for the ss0 do i just define it as:&lt;/P&gt;&lt;P&gt;MX6QDL_PAD_DISP0_DAT23_ECSPI1_SSO&amp;nbsp;&amp;nbsp; 0x100b1&lt;/P&gt;&lt;P&gt;following the same pattern as the other muxes and get rid of the cs-gpios = ... line or is it done differently?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 19:10:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587195#M88808</guid>
      <dc:creator>mmonto58</dc:creator>
      <dc:date>2016-08-09T19:10:37Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Mux - non gpio cs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587196#M88809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi matthew&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according documentation and probe function in linux/drivers/spi/spi-imx.c&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_3.14.28_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/spi/spi-imx.c?h=imx_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/spi/spi-imx.c?h=imx_3.14.28_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;CODE&gt;seems implemented only option with "cs-gpios".&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 01:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587196#M88809</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-10T01:01:00Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Mux - non gpio cs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587197#M88810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that mean that I will have to ask our hardware guys to change the HW for the CS to be a GPIO?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 15:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587197#M88810</guid>
      <dc:creator>mmonto58</dc:creator>
      <dc:date>2016-08-10T15:29:24Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Mux - non gpio cs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587198#M88811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe yes, one can use that pin as gpio and use existing driver&lt;/P&gt;&lt;P&gt;with "cs-gpios".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 01:07:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Mux-non-gpio-cs/m-p/587198#M88811</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-11T01:07:41Z</dc:date>
    </item>
  </channel>
</rss>