<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6Q Encrypted Boot: Key Generation &amp; Blob Creation in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584050#M88595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer chapter 4.11 "High Assurance Boot" of&amp;nbsp; Security Reference Manual for i.MX6 Families of Applications Processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jun 2016 16:33:12 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-06-28T16:33:12Z</dc:date>
    <item>
      <title>iMX6Q Encrypted Boot: Key Generation &amp; Blob Creation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584049#M88594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An explanation of encrypted boot in the document of CST tool is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The encrypted boot case is very similar to generating signed images, but there are two main differences. The first is that the binary image is both decrypted and authenticated using a symmetric key rather than signed using a private asymmetric key. The second is the CST generates a one-time AES Data Encryption Key (DEK) which is used to encrypt the image.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;A cryptographic blob of the DEK must be created during the OEM manufacturing stages on each &lt;/STRONG&gt;&lt;STRONG&gt;processor and then attached to the image on the boot device. The reason for this is the DEK blob &lt;/STRONG&gt;&lt;STRONG&gt;is created using the device unique key embedded into the Freescale processor which is only &lt;/STRONG&gt;&lt;STRONG&gt;readable by the on-chip encryption engine. The DEK is common to all ICs using the same &lt;/STRONG&gt;&lt;STRONG&gt;encrypted image but the DEK blob is unique per IC.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;I assume that it's the bootloader+signature file that is encrypted with DEK. Am I right? &lt;/LI&gt;&lt;LI&gt;CST genrates the DEK. None is generated nor any script exists. Can you please guide me where exactly its done or one should use openssl seperately to generate the key?&lt;/LI&gt;&lt;LI&gt;AES mode: Is it AES-CCM mode?&lt;/LI&gt;&lt;LI&gt;DEK Blob: How to create it?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Greets,&lt;/P&gt;&lt;P&gt;Satya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 13:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584049#M88594</guid>
      <dc:creator>satyadamarla</dc:creator>
      <dc:date>2016-06-28T13:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q Encrypted Boot: Key Generation &amp; Blob Creation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584050#M88595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer chapter 4.11 "High Assurance Boot" of&amp;nbsp; Security Reference Manual for i.MX6 Families of Applications Processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 16:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584050#M88595</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-06-28T16:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q Encrypted Boot: Key Generation &amp; Blob Creation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584051#M88596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply. I am sorry to say some of my questions remain unaswered. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;DEK is generated by CST. My&amp;nbsp; cst-2.3.2. doesn't generate one. Of course I can generate using openssl but as the information on the document suggests (or internet), it's contrary to my trails.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. I think I found a way of to generate the blob, actually a patch: &lt;A href="http://lists.denx.de/pipermail/u-boot/2015-February/204001.html" title="http://lists.denx.de/pipermail/u-boot/2015-February/204001.html"&gt;[U-Boot] [PATCH] imx6: Added DEK blob generator command&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I haven't tried but hope it works. I can only try it after I have clarity about the above step.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Greets,&lt;/P&gt;&lt;P&gt;Satya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jun 2016 09:43:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584051#M88596</guid>
      <dc:creator>satyadamarla</dc:creator>
      <dc:date>2016-06-29T09:43:29Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q Encrypted Boot: Key Generation &amp; Blob Creation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584052#M88597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I hope the following helps &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332147"&gt;Encrypted U-boot Example&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 04:06:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Encrypted-Boot-Key-Generation-Blob-Creation/m-p/584052#M88597</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-06-30T04:06:44Z</dc:date>
    </item>
  </channel>
</rss>