<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: about DCD verification(i.mx6) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-DCD-verification-i-mx6/m-p/583375#M88539</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For Q1, you can think the DCD is a data struct, and it has some special tags. The boot ROM will verify if it is a valid DCD struct for boot up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Q2, that means boot failure happens, it will swicth to serial download mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Aug 2016 04:00:24 GMT</pubDate>
    <dc:creator>qiang_li-mpu_se</dc:creator>
    <dc:date>2016-08-10T04:00:24Z</dc:date>
    <item>
      <title>about DCD verification(i.mx6)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-DCD-verification-i-mx6/m-p/583373#M88537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some questions about DCD verification.&lt;/P&gt;&lt;P&gt;In IMX6SDLRM 8.5.4.3 ECSPI Boot, there is description as bellow.&lt;/P&gt;&lt;P&gt;----------------------------------&lt;/P&gt;&lt;P&gt;The boot ROM code copies 4 KB data from EEPROM device to the internal RAM. If&lt;/P&gt;&lt;P&gt;DCD verification is successful, the ROM code copies the initial 4 KB data, as well as the&lt;/P&gt;&lt;P&gt;rest of the image extracted from application image, directly to the application destination.&lt;/P&gt;&lt;P&gt;---------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1)&lt;/P&gt;&lt;P&gt;Could you tell me the detail of DCD verification(How is the verification done)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q2)&lt;/P&gt;&lt;P&gt;If the DCD verification is failed,what is the next action?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;ZongbiaoLiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 10:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-DCD-verification-i-mx6/m-p/583373#M88537</guid>
      <dc:creator>宗標廖</dc:creator>
      <dc:date>2016-08-09T10:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: about DCD verification(i.mx6)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-DCD-verification-i-mx6/m-p/583374#M88538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Section 8.6.2 [Device Configuration Data (DCD)] of the RM describes&lt;/P&gt;&lt;P&gt;possible restrictions for DCD commands in NOTE comments.&lt;/P&gt;&lt;P&gt;In particular, Table 8-33 (Valid DCD Address Ranges) provides allowed&lt;/P&gt;&lt;P&gt;addresses to access.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If the DCD verification is failed : &lt;BR /&gt;1) Redundant Boot&amp;nbsp; is activated (if enabled) ;&lt;/P&gt;&lt;P&gt;2) SD/MMC Manufacture Mode is entered (section 8.11 SD/MMC Manufacture Mode) ;&lt;/P&gt;&lt;P&gt;3) Serial (USB) bootloader is entered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 03:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-DCD-verification-i-mx6/m-p/583374#M88538</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-10T03:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: about DCD verification(i.mx6)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-DCD-verification-i-mx6/m-p/583375#M88539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For Q1, you can think the DCD is a data struct, and it has some special tags. The boot ROM will verify if it is a valid DCD struct for boot up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For Q2, that means boot failure happens, it will swicth to serial download mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 04:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-DCD-verification-i-mx6/m-p/583375#M88539</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2016-08-10T04:00:24Z</dc:date>
    </item>
  </channel>
</rss>