<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 ​IMX6Q SABRE AUTO ​ CAN Module not working as expected​ on Linux 3.14</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABRE-AUTO-CAN-Module-not-working-as-expected-on-Linux-3/m-p/582067#M88448</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to ​use the ​CAN module​ 1 (CAN1)​​on an ​IMX6​Q SABRE AUTO Board​.​ The followin​g are the list of commands I use to configure CAN1.&lt;/P&gt;&lt;P&gt;&amp;lt; ip link set can1 type can bitrate 250000 sample-point 0.875 loopback off listen-only off triple-sampling on &amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt; ifconfig can1 up &amp;gt;&lt;/P&gt;&lt;P&gt;1. After I configure CAN1 up, I do not see an idle high voltage on the CAN1 DB9 Connector pins(Pin2/Pin7). Why is this so?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. After I press the SW1 (CAN wake-up switch) for a short while, the Pins 2 and 7 go idle high showing default CAN idle state. Can this be handled via any processor pins without using a switch press for the same ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. After i have an IDLE state on the CANH and CANL pins, i tried connecting a can sniffer hardware straight to the CAN1 DB9 connector, but i couldn't see Tx,RX from or to IMX6 CAN1. Is there anything I am missing here ? &lt;/P&gt;&lt;P&gt;I am using the following commands to send and receive,&lt;/P&gt;&lt;P&gt;&amp;lt; cansend can1 123#DEADBEEF &amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt; candump can1 any,0:0,#FFFFFFFF &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. Regarding the termination resistance, i think the SABRE AUTO board uses a 60 ohm termination.My sniffer has a 120 Ohm termination inside. Shouldn't this be compatible as i dont have any long wires between the sniffer connector and the IMX6 CAN connector ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #222222; font-family: arial,sans-serif;"&gt;Any help is appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Aug 2016 06:13:50 GMT</pubDate>
    <dc:creator>shyamjithkv</dc:creator>
    <dc:date>2016-08-09T06:13:50Z</dc:date>
    <item>
      <title>​IMX6Q SABRE AUTO ​ CAN Module not working as expected​ on Linux 3.14</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABRE-AUTO-CAN-Module-not-working-as-expected-on-Linux-3/m-p/582067#M88448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to ​use the ​CAN module​ 1 (CAN1)​​on an ​IMX6​Q SABRE AUTO Board​.​ The followin​g are the list of commands I use to configure CAN1.&lt;/P&gt;&lt;P&gt;&amp;lt; ip link set can1 type can bitrate 250000 sample-point 0.875 loopback off listen-only off triple-sampling on &amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt; ifconfig can1 up &amp;gt;&lt;/P&gt;&lt;P&gt;1. After I configure CAN1 up, I do not see an idle high voltage on the CAN1 DB9 Connector pins(Pin2/Pin7). Why is this so?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. After I press the SW1 (CAN wake-up switch) for a short while, the Pins 2 and 7 go idle high showing default CAN idle state. Can this be handled via any processor pins without using a switch press for the same ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. After i have an IDLE state on the CANH and CANL pins, i tried connecting a can sniffer hardware straight to the CAN1 DB9 connector, but i couldn't see Tx,RX from or to IMX6 CAN1. Is there anything I am missing here ? &lt;/P&gt;&lt;P&gt;I am using the following commands to send and receive,&lt;/P&gt;&lt;P&gt;&amp;lt; cansend can1 123#DEADBEEF &amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt; candump can1 any,0:0,#FFFFFFFF &amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. Regarding the termination resistance, i think the SABRE AUTO board uses a 60 ohm termination.My sniffer has a 120 Ohm termination inside. Shouldn't this be compatible as i dont have any long wires between the sniffer connector and the IMX6 CAN connector ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #222222; font-family: arial,sans-serif;"&gt;Any help is appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 06:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABRE-AUTO-CAN-Module-not-working-as-expected-on-Linux-3/m-p/582067#M88448</guid>
      <dc:creator>shyamjithkv</dc:creator>
      <dc:date>2016-08-09T06:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: ​IMX6Q SABRE AUTO ​ CAN Module not working as expected​ on Linux 3.14</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABRE-AUTO-CAN-Module-not-working-as-expected-on-Linux-3/m-p/582068#M88449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi shyamjith&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;flexcan testing general steps are described in&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1437"&gt;All Boards FlexCAN&lt;/A&gt;&lt;/P&gt;&lt;P&gt;for i.MX6 recommended to use imx-test package,&amp;nbsp; folder /test/can&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.3.tar.gz" target="test_blank"&gt;www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.3.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 00:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABRE-AUTO-CAN-Module-not-working-as-expected-on-Linux-3/m-p/582068#M88449</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-11T00:45:58Z</dc:date>
    </item>
  </channel>
</rss>