<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Avilavility of i.MX6S PCIeGEN2 port in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581337#M88410</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PCIe port of the i.MX6Solo processor is compliant with the PCIe Gen.2 specification at the speeds of up to 5Gbit/s. So, there should be no any problem.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Sep 2016 10:07:04 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-09-01T10:07:04Z</dc:date>
    <item>
      <title>Avilavility of i.MX6S PCIeGEN2 port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581336#M88409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have plan to use mSATA or CFast devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to connect them to the i.MX6S PCIeGEN2 port?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I only concern about physical layer and I do not mention about drivers at this point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any difficulty for it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 03:43:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581336#M88409</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2016-09-01T03:43:37Z</dc:date>
    </item>
    <item>
      <title>Re: Avilavility of i.MX6S PCIeGEN2 port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581337#M88410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PCIe port of the i.MX6Solo processor is compliant with the PCIe Gen.2 specification at the speeds of up to 5Gbit/s. So, there should be no any problem.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 10:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581337#M88410</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-09-01T10:07:04Z</dc:date>
    </item>
    <item>
      <title>Re: Avilavility of i.MX6S PCIeGEN2 port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581338#M88411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Autur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just in case, I want to confirm one more time.&lt;/P&gt;&lt;P&gt;I checked pin assignment of mPCIe nad mSATA. Please see attached materials.&lt;/P&gt;&lt;P&gt;As far as I know, some PCs actually has dual roll slot(mPCIe and mSATA).&lt;/P&gt;&lt;P&gt;Does i.MX6DL-SabreSD also support both?&lt;/P&gt;&lt;P&gt;In another word, does i.MX6 PCIe support SATA I/F too?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="mPCIe_mSATA52_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2858iC4A9125A68F7FB3F/image-size/large?v=v2&amp;amp;px=999" role="button" title="mPCIe_mSATA52_2.png" alt="mPCIe_mSATA52_2.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="mPCIe_mSATA52.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2898i56C1F9D78705EBB0/image-size/large?v=v2&amp;amp;px=999" role="button" title="mPCIe_mSATA52.png" alt="mPCIe_mSATA52.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 09:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581338#M88411</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2016-09-02T09:01:47Z</dc:date>
    </item>
    <item>
      <title>Re: Avilavility of i.MX6S PCIeGEN2 port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581339#M88412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, the Mini-PCIe connector of the i.MX6DL SABRE SD board does not support Mini-SATA. There is a separate SATA connector on the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Sep 2016 08:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Avilavility-of-i-MX6S-PCIeGEN2-port/m-p/581339#M88412</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-09-05T08:05:31Z</dc:date>
    </item>
  </channel>
</rss>