<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックNo MIPI DSI clock available</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-MIPI-DSI-clock-available/m-p/581129#M88401</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to run a MIPI DSI display on savageboard-quad of which processor is imx6q. I am using the Yocto release provided by saveboard site. Kernel Version is 3.0.35. I have enabled MIPI DSI host controller driver and Himax HX8369A MIPI DSI panel in Kernel configuration. I am using Himax HX8394F MIPI DSI panel. So I ported current&amp;nbsp; HX8369A code for HX8394F.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see that the driver is probed and initialized in the kernel logs. But LCD_ID is not read at all. I got 0x00 for LCD_ID. I analyzed the signals with scope. Data lane signals seem to have expected waveforms. But MIPI DSI clock signals are not as I would expect. Both have 1V DC for a long time, than it toggles, and goes back to 0V and stay still.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be the reason beyond No MIPI DSI clock issue? I tried to trace video_27m_clk_root in the kernel, but no clue at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Seniz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Aug 2016 10:59:41 GMT</pubDate>
    <dc:creator>senizhuseyin</dc:creator>
    <dc:date>2016-08-08T10:59:41Z</dc:date>
    <item>
      <title>No MIPI DSI clock available</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-MIPI-DSI-clock-available/m-p/581129#M88401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to run a MIPI DSI display on savageboard-quad of which processor is imx6q. I am using the Yocto release provided by saveboard site. Kernel Version is 3.0.35. I have enabled MIPI DSI host controller driver and Himax HX8369A MIPI DSI panel in Kernel configuration. I am using Himax HX8394F MIPI DSI panel. So I ported current&amp;nbsp; HX8369A code for HX8394F.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see that the driver is probed and initialized in the kernel logs. But LCD_ID is not read at all. I got 0x00 for LCD_ID. I analyzed the signals with scope. Data lane signals seem to have expected waveforms. But MIPI DSI clock signals are not as I would expect. Both have 1V DC for a long time, than it toggles, and goes back to 0V and stay still.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be the reason beyond No MIPI DSI clock issue? I tried to trace video_27m_clk_root in the kernel, but no clue at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Seniz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 10:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-MIPI-DSI-clock-available/m-p/581129#M88401</guid>
      <dc:creator>senizhuseyin</dc:creator>
      <dc:date>2016-08-08T10:59:41Z</dc:date>
    </item>
  </channel>
</rss>