<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMIPI DSI max display resolution</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-max-display-resolution/m-p/580938#M88383</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the maximum display resolution for MIPI DSI?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it 1280x720 (as it is mentioned in IMX6DQRM Rev. 3, 07/2015) or is it 1024x768 (IMX6QLXRM Rev L3.0.35_4.1.0, 09/2013)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to connect the 1280x720 Super AMOLED display to our IMX6Q board, and we wonder if it has any chance to work correctly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jul 2016 08:03:12 GMT</pubDate>
    <dc:creator>jotes</dc:creator>
    <dc:date>2016-07-18T08:03:12Z</dc:date>
    <item>
      <title>MIPI DSI max display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-max-display-resolution/m-p/580938#M88383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the maximum display resolution for MIPI DSI?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it 1280x720 (as it is mentioned in IMX6DQRM Rev. 3, 07/2015) or is it 1024x768 (IMX6QLXRM Rev L3.0.35_4.1.0, 09/2013)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would like to connect the 1280x720 Super AMOLED display to our IMX6Q board, and we wonder if it has any chance to work correctly?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jul 2016 08:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-max-display-resolution/m-p/580938#M88383</guid>
      <dc:creator>jotes</dc:creator>
      <dc:date>2016-07-18T08:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI DSI max display resolution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-max-display-resolution/m-p/580939#M88384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The maximum possible display resolution on the MIPI DSI interface of the i.MX6Dual/Quad processors is 1280x720 pixels, as specified in the Reference Manual document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 09:39:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-max-display-resolution/m-p/580939#M88384</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-07-27T09:39:55Z</dc:date>
    </item>
  </channel>
</rss>