<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX7D :  Which pin do I use for inputting external clock signal ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579691#M88327</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; check the IMX7DSHDG .&lt;/P&gt;&lt;P&gt;In User's Guide IMX7DSHDG Rev. 0 , 4.3. Checking for clock pitfalls,&lt;/P&gt;&lt;P&gt;it is described that&lt;/P&gt;&lt;P&gt;CLK1_P/N/CLK2 can be used as oscillator inputs for low jitter special frequency sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;/P&gt;&lt;P&gt;Is it possible to use the CLK1_P/N/CLK2 as PLL reference clock ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Aug 2016 01:39:02 GMT</pubDate>
    <dc:creator>koichisakagami</dc:creator>
    <dc:date>2016-08-10T01:39:02Z</dc:date>
    <item>
      <title>iMX7D :  Which pin do I use for inputting external clock signal ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579689#M88325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;BR /&gt;We have been developing our product with iMX7D.&lt;BR /&gt;I have a question about&amp;nbsp; iMX7D PIN name for inputting external clock signal .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Reference Manual IMX7DRM Rev. 0 , 5.3.2 Functional Description,&lt;BR /&gt;it is described that &lt;BR /&gt;Crystal oscillator provides selection control switches to either select crystal clock or&lt;BR /&gt;external clock through PADI pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Which is the PADI pin ?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Is it XTALI pin ?&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Or are they CCM_CLK1_P/CCM_CLK1_N , CCM_CLK2 pin ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards, &lt;BR /&gt;Koichi Sakagami &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 09:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579689#M88325</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2016-08-08T09:01:59Z</dc:date>
    </item>
    <item>
      <title>Re: iMX7D :  Which pin do I use for inputting external clock signal ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579690#M88326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; From the i.MX7 hardware design guide : "External kilohertz source If feeding an&lt;/P&gt;&lt;P&gt;external clock into the device, RTC_XTALI can be driven DC-coupled with RTC_XTALO&lt;/P&gt;&lt;P&gt;floated or driven with a complimentary signal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The voltage level of this driving clock should not exceed the voltage of VDD_SNVS_CAP &lt;BR /&gt;and the frequency should be &amp;lt;100 kHz under typical conditions. Do not exceed VDD_SNVS_CAP &lt;BR /&gt;or damage/malfunction may occur. The RTC_XTALI signal should not be driven if the VDD_SNVS_CAP &lt;BR /&gt;supply is off. This can lead to damage or malfunction.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; For RTC_XTALI VIL and VIH voltage levels, see the latest i.MX 7 series datasheet available &lt;BR /&gt;at nxp.com. Note that if this external clock is stopped, the internal ring oscillator starts automatically."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf" title="http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf"&gt;http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 05:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579690#M88326</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-09T05:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX7D :  Which pin do I use for inputting external clock signal ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579691#M88327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yuri,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; check the IMX7DSHDG .&lt;/P&gt;&lt;P&gt;In User's Guide IMX7DSHDG Rev. 0 , 4.3. Checking for clock pitfalls,&lt;/P&gt;&lt;P&gt;it is described that&lt;/P&gt;&lt;P&gt;CLK1_P/N/CLK2 can be used as oscillator inputs for low jitter special frequency sources.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;/P&gt;&lt;P&gt;Is it possible to use the CLK1_P/N/CLK2 as PLL reference clock ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 01:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579691#M88327</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2016-08-10T01:39:02Z</dc:date>
    </item>
    <item>
      <title>Re: iMX7D :  Which pin do I use for inputting external clock signal ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579692#M88328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From i.MX7 RM :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; "Both CLK1P/N and CLK2 can take input clocks from outside of the SoC and provide&lt;/P&gt;&lt;P&gt;them to the PLLs or to the other modules, or they can take the outputs of the PLLs and&lt;/P&gt;&lt;P&gt;provide them outside of the SoC as a functional or reference clock."&lt;/P&gt;&lt;P&gt;&amp;nbsp; "Reference input clock for any of the PLLs could be selected individually by the&lt;/P&gt;&lt;P&gt;BYPASS_CLK_SRC feed of the PLL control register. Each PLL can use one of the&lt;/P&gt;&lt;P&gt;following clock source as its reference clock:&lt;/P&gt;&lt;P&gt;• 24MHz clock from XTAL.&lt;/P&gt;&lt;P&gt;• External reference clock from CLK1P/N.&lt;/P&gt;&lt;P&gt;• External reference clock from CLK2."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 03:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-Which-pin-do-I-use-for-inputting-external-clock-signal/m-p/579692#M88328</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-10T03:01:54Z</dc:date>
    </item>
  </channel>
</rss>