<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Booting issue for imx283</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-for-imx283/m-p/579656#M88315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aditya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;restarting can be caused by brownouts, so one can tweak&lt;/P&gt;&lt;P&gt;levels using HW_POWER_xx[BO_OFFSET] settings or&lt;/P&gt;&lt;P&gt;ddr errors, one can run ddr tests on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/375692#375692"&gt;https://community.freescale.com/message/375692#375692&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Sep 2016 00:42:44 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-09-02T00:42:44Z</dc:date>
    <item>
      <title>Booting issue for imx283</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-for-imx283/m-p/579655#M88314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Booting issue for imx283&lt;/P&gt;&lt;P&gt;Following is the log.&lt;/P&gt;&lt;P&gt;The kernel is linux-2.6.35.3&lt;/P&gt;&lt;P&gt;After the&amp;nbsp;&lt;/P&gt;&lt;P&gt;finish boot prep,start to run ...&lt;/P&gt;&lt;P&gt;it restarts....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NAND read: device 0 offset 0x200000, size 0x300000&lt;BR /&gt; 3145728 bytes read: OK&lt;BR /&gt;## Booting kernel from Legacy Image at 42000000 ...&lt;BR /&gt; Image Name: Linux-2.6.35.3-571-gcca29a0&lt;BR /&gt; Image Type: ARM Linux Kernel Image (uncompressed)&lt;BR /&gt; Data Size: 2329996 Bytes = 2.2 MB&lt;BR /&gt; Load Address: 40008000&lt;BR /&gt; Entry Point: 40008000&lt;BR /&gt; Verifying Checksum ... OK&lt;BR /&gt; Loading Kernel Image ... OK&lt;BR /&gt;OK&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;Linux version 2.6.35.3-571-gcca29a0 (aditya@aditya-PC) (gcc version 4.4.4 (4.4.4_09.06.2010) ) #4 PREEMPT Thu Sep 1 16:39:28 CST 2016&lt;BR /&gt;CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177&lt;BR /&gt;CPU: VIVT data cache, VIVT instruction cache&lt;BR /&gt;Machine: Freescale MX28EVK board&lt;BR /&gt;Memory policy: ECC disabled, Data cache writeback&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512&lt;BR /&gt;Kernel command line: gpmi=g console=ttyAM0,115200n8 ubi.mtd=5 root=ubi0:rootfs rootfstype=ubifs ro mem=128M&lt;BR /&gt;PID hash table entries: 512 (order: -1, 2048 bytes)&lt;BR /&gt;Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)&lt;BR /&gt;Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)&lt;BR /&gt;Memory: 128MB = 128MB total&lt;BR /&gt;Memory: 124840k/124840k available, 6232k reserved, 0K highmem&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)&lt;BR /&gt; DMA : 0xfde00000 - 0xffe00000 ( 32 MB)&lt;BR /&gt; vmalloc : 0xc8800000 - 0xf0000000 ( 632 MB)&lt;BR /&gt; lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)&lt;BR /&gt; modules : 0xbf000000 - 0xc0000000 ( 16 MB)&lt;BR /&gt; .init : 0xc0008000 - 0xc002f000 ( 156 kB)&lt;BR /&gt; .text : 0xc002f000 - 0xc0480000 (4420 kB)&lt;BR /&gt; .data : 0xc0480000 - 0xc04b39c0 ( 207 kB)&lt;BR /&gt;SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;BR /&gt;Hierarchical RCU implementation.&lt;BR /&gt; RCU-based detection of stalled CPUs is disabled.&lt;BR /&gt; Verbose stalled-CPUs detection is disabled.&lt;BR /&gt;NR_IRQS:288&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;console [ttyAM0] enabled&lt;BR /&gt;Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Security Framework initialized&lt;BR /&gt;SELinux: Initializing.&lt;BR /&gt;Mount-cache hash table entries: 512&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;regulator: core version 0.5&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;regulator: vddd: 800 &amp;lt;--&amp;gt; 1575 mV at 1500 mV fast normal &lt;BR /&gt;regulator: vdddbo: 800 &amp;lt;--&amp;gt; 1575 mV fast normal &lt;BR /&gt;regulator: vdda: 1500 &amp;lt;--&amp;gt; 2275 mV at 1800 mV fast normal &lt;BR /&gt;vddio = 3380000, val=10&lt;BR /&gt;regulator: vddio: 2880 &amp;lt;--&amp;gt; 3680 mV at 3380 mV fast normal &lt;BR /&gt;regulator: overall_current: fast normal &lt;BR /&gt;regulator: vbus5v: &lt;BR /&gt;regulator: mxs-duart-1: fast normal &lt;BR /&gt;regulator: mxs-bl-1: fast normal &lt;BR /&gt;regulator: mxs-i2c-1: fast normal &lt;BR /&gt;regulator: mmc_ssp-1: fast normal &lt;BR /&gt;regulator: mmc_ssp-2: fast normal &lt;BR /&gt;regulator: charger-1: fast normal &lt;BR /&gt;regulator: power-test-1: fast normal &lt;BR /&gt;regulator: cpufreq-1: fast normal &lt;BR /&gt;**kernel for EasyARM-i.MX283 &lt;BR /&gt;i.MX IRAM pool: 120 KB@0xc8820000&lt;BR /&gt;Initializing GPMI pins&lt;BR /&gt;add device pwm chanel 4&lt;BR /&gt;add device pwm chanel 7&lt;BR /&gt;usb DR wakeup device is registered&lt;BR /&gt;IMX usb wakeup probe&lt;BR /&gt;audit: cannot initialize inotify handle&lt;BR /&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;Freescale USB OTG Driver loaded, $Revision: 1.55 $&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;Switching to clocksource mxs clock source&lt;BR /&gt;Boot process: init&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP route cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;TCP established hash table entries: 4096 (order: 3, 32768 bytes)&lt;BR /&gt;TCP bind hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 4096 bind 4096)&lt;BR /&gt;TCP reno registered&lt;BR /&gt;UDP hash table entries: 256 (order: 0, 4096 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;IMX usb wakeup probe&lt;BR /&gt;usb h1 wakeup device is registered&lt;BR /&gt;mxs_cpu_init: cpufreq init finished&lt;BR /&gt;audit: initializing netlink socket (disabled)&lt;BR /&gt;type=2000 audit(0.580:1): initialized&lt;BR /&gt;VFS: Disk quotas dquot_6.5.2&lt;BR /&gt;Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;BR /&gt;JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.&lt;BR /&gt;msgmni has been set to 243&lt;BR /&gt;alg: No test for stdrng (krng)&lt;BR /&gt;cryptodev: driver loaded.&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;baclight_device easy283-pwm.4 register succcessed &lt;BR /&gt;init_pwm ch 4&lt;BR /&gt;baclight_device easy283-pwm.7 register succcessed &lt;BR /&gt;init_pwm ch 7&lt;BR /&gt;set dclk 8000000 Hz,real lcd clk=8000000 Hz&lt;BR /&gt;Console: switching to colour frame buffer device 60x34&lt;BR /&gt;set dclk 8000000 Hz,real lcd clk=8000000 Hz&lt;BR /&gt;mxs-duart.0: ttyAM0 at MMIO 0x80074000 (irq = 47) is a DebugUART&lt;BR /&gt;mxs-auart.0: ttySP0 at MMIO 0x8006a000 (irq = 112) is a mxs-auart.0&lt;BR /&gt;Found APPUART 3.1.0&lt;BR /&gt;mxs-auart.1: ttySP1 at MMIO 0x8006c000 (irq = 113) is a mxs-auart.1&lt;BR /&gt;Found APPUART 3.1.0&lt;BR /&gt;mxs-auart.2: ttySP2 at MMay 18 201510:14:49&lt;BR /&gt;finish boot prep,start to run ...&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2009.08-dirty ( 5��月 18 2015 - 10:22:36)&lt;/P&gt;&lt;P&gt;Freescale i.MX28 family&lt;BR /&gt;CPU: 454 MHz&lt;BR /&gt;BUS: 151 MHz&lt;BR /&gt;EMI: 205 MHz&lt;BR /&gt;GPMI: 24 MHz&lt;BR /&gt;DRAM: 128 MB&lt;BR /&gt;NAND: proton id: c2 f1 80 1d c2 f1&lt;BR /&gt;mfr_id: c2 &lt;BR /&gt;nand_device_info_fn_mx called.&lt;BR /&gt;nand slc&lt;BR /&gt;Manufacturer : Unknown (0xc2)&lt;BR /&gt;Device Code : 0xf1&lt;BR /&gt;Cell Technology : SLC&lt;BR /&gt;Chip Size : 128 MiB&lt;BR /&gt;Pages per Block : 64&lt;BR /&gt;Page Geometry : 2048+64&lt;BR /&gt;ECC Strength : 4 bits&lt;BR /&gt;ECC Size : 512 B&lt;BR /&gt;Data Setup Time : 20 ns&lt;BR /&gt;Data Hold Time : 10 ns&lt;BR /&gt;Address Setup Time: 20 ns&lt;BR /&gt;GPMI Sample Delay : 6 ns&lt;BR /&gt;tREA : Unknown&lt;BR /&gt;tRLOH : Unknown&lt;BR /&gt;tRHOH : Unknown&lt;BR /&gt;Description : MX30LF1G08&lt;BR /&gt;128 MiB&lt;BR /&gt;MMC: IMX_SSP_MMC: 0, IMX_SSP_MMC: 1&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: fec_get_mac_addr&lt;BR /&gt;FEC0&lt;BR /&gt;Hit any key to stop autoboot:: 0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 08:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-for-imx283/m-p/579655#M88314</guid>
      <dc:creator>adityapatil</dc:creator>
      <dc:date>2016-09-01T08:51:22Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue for imx283</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-for-imx283/m-p/579656#M88315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aditya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;restarting can be caused by brownouts, so one can tweak&lt;/P&gt;&lt;P&gt;levels using HW_POWER_xx[BO_OFFSET] settings or&lt;/P&gt;&lt;P&gt;ddr errors, one can run ddr tests on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/375692#375692"&gt;https://community.freescale.com/message/375692#375692&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 00:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-for-imx283/m-p/579656#M88315</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-02T00:42:44Z</dc:date>
    </item>
    <item>
      <title>Re: Booting issue for imx283</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-for-imx283/m-p/579657#M88316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I actually used the ( uboot + uImage + rootfs) update tool called mfgtool.&lt;/P&gt;&lt;P&gt;Problem solved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;- Aditya&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 02:26:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Booting-issue-for-imx283/m-p/579657#M88316</guid>
      <dc:creator>adityapatil</dc:creator>
      <dc:date>2016-09-13T02:26:54Z</dc:date>
    </item>
  </channel>
</rss>