<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6ul emmc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-emmc/m-p/578141#M88192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 小辉哥,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 你上面给出来的列表不完整，BOOT_CFG1[7:5]仅仅是用来确定是从哪个类型的接口启动，比如你的BOOT_CFG1[7：5]=011，表示从uSDHC接口启动，你还要选择是uSDHC1 or uSDHC2口（要配置BOOT_CFG2[4:3]=00---uSDHC1或者BOOT_CFG2[4:3]=01---uSDHC2），这要看你的eMMC是接在哪个uSDHC口上了；请按照下面的配置试试，我假设你接在了uSDHC2口上：&lt;/P&gt;&lt;P&gt;（1）调整配置为：&lt;/P&gt;&lt;P&gt;BOOT_CFG1[7:5]=011---选择uSDHC接口&lt;/P&gt;&lt;P&gt;BOOT_CFG2[4:3]=01----使用uSDHC2的eMMC启动&lt;/P&gt;&lt;P&gt;BOOT_CFG2[5]=0--------使用eMMC协议&lt;/P&gt;&lt;P&gt;BOOT_CFG2[7:6]=01----使用8bit模式&lt;/P&gt;&lt;P&gt;BOOT_CFG4[4]=0--------BT_FUSE_SEL=0，表示由外部GPIO控制启动，而不是eFUSE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BOOT_MODE[1:0]=10---表示从板上Flash启动系统，而不是USB OTG接口。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;（2）烧写问题&lt;/P&gt;&lt;P&gt;如果上述的配置，还不能启动系统，那么请你调整一下MFG TOOLS的ucl2.xml的list，让它只烧写u-boot到eMMC中，其他的image烧写行暂时注释掉，然后再尝试启动板子，看是不是能够起来。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;（3）可能的问题&lt;/P&gt;&lt;P&gt;针对（1）中的配置，可以在reference manual中，再核对一下板子的启动配置是否正确，再做启动尝试。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;一般来说，上面的情况应该可以解决目前的问题！&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;伟东&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Aug 2016 08:30:59 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2016-08-10T08:30:59Z</dc:date>
    <item>
      <title>imx6ul emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-emmc/m-p/578140#M88191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你们好，我参考官方的imx6ul-evk设计一个板子 想使用emmc启动，我修改了uboot和dts 现在代码可以下载成功，但是就是不启动，启动模式也是设置为emmc启动&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1874i416B3621DDE9705A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 08:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-emmc/m-p/578140#M88191</guid>
      <dc:creator>小辉哥</dc:creator>
      <dc:date>2016-08-09T08:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ul emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-emmc/m-p/578141#M88192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi 小辉哥,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 你上面给出来的列表不完整，BOOT_CFG1[7:5]仅仅是用来确定是从哪个类型的接口启动，比如你的BOOT_CFG1[7：5]=011，表示从uSDHC接口启动，你还要选择是uSDHC1 or uSDHC2口（要配置BOOT_CFG2[4:3]=00---uSDHC1或者BOOT_CFG2[4:3]=01---uSDHC2），这要看你的eMMC是接在哪个uSDHC口上了；请按照下面的配置试试，我假设你接在了uSDHC2口上：&lt;/P&gt;&lt;P&gt;（1）调整配置为：&lt;/P&gt;&lt;P&gt;BOOT_CFG1[7:5]=011---选择uSDHC接口&lt;/P&gt;&lt;P&gt;BOOT_CFG2[4:3]=01----使用uSDHC2的eMMC启动&lt;/P&gt;&lt;P&gt;BOOT_CFG2[5]=0--------使用eMMC协议&lt;/P&gt;&lt;P&gt;BOOT_CFG2[7:6]=01----使用8bit模式&lt;/P&gt;&lt;P&gt;BOOT_CFG4[4]=0--------BT_FUSE_SEL=0，表示由外部GPIO控制启动，而不是eFUSE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BOOT_MODE[1:0]=10---表示从板上Flash启动系统，而不是USB OTG接口。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;（2）烧写问题&lt;/P&gt;&lt;P&gt;如果上述的配置，还不能启动系统，那么请你调整一下MFG TOOLS的ucl2.xml的list，让它只烧写u-boot到eMMC中，其他的image烧写行暂时注释掉，然后再尝试启动板子，看是不是能够起来。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;（3）可能的问题&lt;/P&gt;&lt;P&gt;针对（1）中的配置，可以在reference manual中，再核对一下板子的启动配置是否正确，再做启动尝试。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;一般来说，上面的情况应该可以解决目前的问题！&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;伟东&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 08:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-emmc/m-p/578141#M88192</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-08-10T08:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ul emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-emmc/m-p/578142#M88193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi 伟东，&lt;/P&gt;&lt;P&gt;你说的是对的，这样设置是正确的，只是我的电平状态不对，高电平只有1.2V左右 我换了小电阻就ok了，谢谢你。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 11:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-emmc/m-p/578142#M88193</guid>
      <dc:creator>小辉哥</dc:creator>
      <dc:date>2016-08-11T11:23:42Z</dc:date>
    </item>
  </channel>
</rss>