<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IPU: how to stop a task?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IPU-how-to-stop-a-task/m-p/577570#M88128</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for the response, but I tried this already by the&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; # devmem 0x02a000dc w $[ (1&amp;lt;&amp;lt;31) | ((1&amp;lt;&amp;lt;23) - 1) ]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;stated above.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Sep 2016 09:24:46 GMT</pubDate>
    <dc:creator>ensc</dc:creator>
    <dc:date>2016-09-21T09:24:46Z</dc:date>
    <item>
      <title>IPU: how to stop a task?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-how-to-stop-a-task/m-p/577568#M88126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a driver which uses the IPU to rotate an image.&amp;nbsp; Things are working usually fine, but it happens that after stopping this operation, the corresponding pre-processor task is stuck in the active state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;E.g. when reading IPU_PROC_TASK_STAT, the corresponding bit is always set&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; # devmem 0x02a00250&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000100&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to clear IPU_IC_CONF (base + 0x20000), IPU_CONF (base + 0) and even wiping whole IPU memory by&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; # devmem 0x02a000dc w $[ (1&amp;lt;&amp;lt;31) | ((1&amp;lt;&amp;lt;23) - 1) ]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this does not help, task still stays in ACTIVE state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the recommended way to reset tasks?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 11:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-how-to-stop-a-task/m-p/577568#M88126</guid>
      <dc:creator>ensc</dc:creator>
      <dc:date>2016-08-08T11:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: IPU: how to stop a task?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-how-to-stop-a-task/m-p/577569#M88127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can refer to the Memory Reset Control Register (IPUx_MEM_RST) in the mx6 Reference Manunal, This register controls the memory reset mechanism. IPU has a hardware mechanism for&lt;BR /&gt;clearing the content of the internal memories. This allows the user to clear the content of&lt;BR /&gt;or more of the internal memories without the need to perform write accesses to the&lt;BR /&gt;memories.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 09:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-how-to-stop-a-task/m-p/577569#M88127</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-09-21T09:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: IPU: how to stop a task?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-how-to-stop-a-task/m-p/577570#M88128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for the response, but I tried this already by the&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; # devmem 0x02a000dc w $[ (1&amp;lt;&amp;lt;31) | ((1&amp;lt;&amp;lt;23) - 1) ]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;stated above.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 09:24:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-how-to-stop-a-task/m-p/577570#M88128</guid>
      <dc:creator>ensc</dc:creator>
      <dc:date>2016-09-21T09:24:46Z</dc:date>
    </item>
  </channel>
</rss>