<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LTIB MX35 misses amd-gpu module in 2.6.31 kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-MX35-misses-amd-gpu-module-in-2-6-31-kernel/m-p/150074#M881</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got a reply from Freescale that version 102010 and 112011 don't support the i.MX35.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I didn't get an answer on the GPU support yet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Mar 2011 08:48:28 GMT</pubDate>
    <dc:creator>udragon</dc:creator>
    <dc:date>2011-03-08T08:48:28Z</dc:date>
    <item>
      <title>LTIB MX35 misses amd-gpu module in 2.6.31 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-MX35-misses-amd-gpu-module-in-2-6-31-kernel/m-p/150073#M880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm building a rootfs based upon ltib v﻿﻿﻿L2.6.31_09.12.01 for the MX35 3stack EVK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I deploy the rootfs there's no gpu.o/gpu.ko available.&lt;/P&gt;&lt;P&gt;Also in the kernel config there's no option to enable -kernel- GPU support&lt;/P&gt;&lt;P&gt;(The userspace packages&amp;nbsp;amd-gpu-bin-mx35 and libz160-bin are both enabled so there's no issue there)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In version 10.2010 of ltib, using L2.6.35, there is a&amp;nbsp;MXC_AMD_GPU option available, however the IPU build for MX35 in this LTIB version is broken so I can't use that LTIB version either.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did any of you manage to enable the amd-gpu kernel driver for MX35 with ltib ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2011 12:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-MX35-misses-amd-gpu-module-in-2-6-31-kernel/m-p/150073#M880</guid>
      <dc:creator>udragon</dc:creator>
      <dc:date>2011-03-03T12:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB MX35 misses amd-gpu module in 2.6.31 kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-MX35-misses-amd-gpu-module-in-2-6-31-kernel/m-p/150074#M881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got a reply from Freescale that version 102010 and 112011 don't support the i.MX35.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I didn't get an answer on the GPU support yet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2011 08:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-MX35-misses-amd-gpu-module-in-2-6-31-kernel/m-p/150074#M881</guid>
      <dc:creator>udragon</dc:creator>
      <dc:date>2011-03-08T08:48:28Z</dc:date>
    </item>
  </channel>
</rss>