<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: run bootcmd_obds in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/run-bootcmd-obds/m-p/186278#M8805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Thanks much for the link. I downloaded the code and located the section that exactly explains the behavior of the "run bootcmd_obds" described above. I imagine bootcmd_obds is something that was added to the Linux image that ships with the MCIMX53-START-R reference board.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Sep 2012 21:45:14 GMT</pubDate>
    <dc:creator>marek1z</dc:creator>
    <dc:date>2012-09-06T21:45:14Z</dc:date>
    <item>
      <title>run bootcmd_obds</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/run-bootcmd-obds/m-p/186276#M8803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have the MCIMX53-START-R dev board. We built our own board using the dev board’s reference design.&lt;/P&gt;&lt;P&gt;We are able to boot our board using the boot image that came with the dev board on an SD card and execute “run bootcmd_obds”.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have observed the following behavior:&lt;/P&gt;&lt;P&gt;When executing “run bootcmd_obds” for the first time, the tools don’t actually run the diagnostic tests. The system appears to hang – I assume this is expected as the tools probably expected things setup for the dev board. Executing the above command however does program general purpose fuses&lt;/P&gt;&lt;P&gt;0x63F9887C = 0x0C and 0x63F98878 = 0x00.&lt;/P&gt;&lt;P&gt;When executing “run bootcmd_obds” for the second time, the tools still don’t run the diagnostic tests. Instead, the system appears to hang as before and the general purpose fuse is set: 0x63F98878 = 0x01.&lt;/P&gt;&lt;P&gt;When executing “run bootcmd_obds” for the third time, the tools actually run.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to find out what else the OBDS does to the fuse map when run for the first/second time on our board. I am happy to study the source code. This is where I need help.&lt;/P&gt;&lt;P&gt;What actually runs when the command “run bootcmd_obds” is executed?&lt;/P&gt;&lt;P&gt;Where do I find the source code for what runs?&lt;/P&gt;&lt;P&gt;Can anyone familiar with OBDS briefly summarize the fuse changes that take place when the above command is executed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2012 21:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/run-bootcmd-obds/m-p/186276#M8803</guid>
      <dc:creator>marek1z</dc:creator>
      <dc:date>2012-09-04T21:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: run bootcmd_obds</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/run-bootcmd-obds/m-p/186277#M8804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I don't know where this command comes from, and wasn't able to identify it in u-boot sources.&lt;/P&gt;&lt;P&gt;OBDS targets Freescale reference boards, and as part of the test procedure, it will typically blow the rev of the board in fuses.&lt;/P&gt;&lt;P&gt;As the test code is probably not totally adapted to your board, I rather suggest to download the &lt;A href="https://www.freescale.com/webapp/Download?colCode=IMX53_QSB_OBDS&amp;amp;appType=license&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Lab%20and%20Test%20Software&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=zip&amp;amp;WT_ASSET=Downloads&amp;amp;sr=60&amp;amp;Parent_nodeId=1286482399115734638749&amp;amp;Parent_pageType=product" target="_blank"&gt;IMX53_QSB_OBDS&lt;/A&gt; code for the Freescale web site, and make the necessary adjustment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2012 10:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/run-bootcmd-obds/m-p/186277#M8804</guid>
      <dc:creator>FlorentAuger</dc:creator>
      <dc:date>2012-09-06T10:13:29Z</dc:date>
    </item>
    <item>
      <title>Re: run bootcmd_obds</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/run-bootcmd-obds/m-p/186278#M8805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Thanks much for the link. I downloaded the code and located the section that exactly explains the behavior of the "run bootcmd_obds" described above. I imagine bootcmd_obds is something that was added to the Linux image that ships with the MCIMX53-START-R reference board.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2012 21:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/run-bootcmd-obds/m-p/186278#M8805</guid>
      <dc:creator>marek1z</dc:creator>
      <dc:date>2012-09-06T21:45:14Z</dc:date>
    </item>
  </channel>
</rss>