<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCIe line impedance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-line-impedance/m-p/576333#M88037</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PCIe to communicate between an IMX6 and IGLOO2 FPGA, both mounted on the same PCB.&lt;/P&gt;&lt;P&gt;The IMX6 hardware development manual says to route PICe at 85 ohms differential impedance, yet the SABRE_SD evaluation board, IMX6 REX and other designs I have seen all route PCIe lines at 100 ohm differential.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The IGLOO2 can terminate to 80, 100 or 120 ohm differential, should I use 85 or 100 ohm impedance lines?&lt;/P&gt;&lt;P&gt;Can anyone explain why the hardware development guide says 85 ohms yet everyone else seems to use 100 ohm lines?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dominic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jul 2016 10:05:45 GMT</pubDate>
    <dc:creator>dominicmusgrove</dc:creator>
    <dc:date>2016-07-15T10:05:45Z</dc:date>
    <item>
      <title>PCIe line impedance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-line-impedance/m-p/576333#M88037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PCIe to communicate between an IMX6 and IGLOO2 FPGA, both mounted on the same PCB.&lt;/P&gt;&lt;P&gt;The IMX6 hardware development manual says to route PICe at 85 ohms differential impedance, yet the SABRE_SD evaluation board, IMX6 REX and other designs I have seen all route PCIe lines at 100 ohm differential.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The IGLOO2 can terminate to 80, 100 or 120 ohm differential, should I use 85 or 100 ohm impedance lines?&lt;/P&gt;&lt;P&gt;Can anyone explain why the hardware development guide says 85 ohms yet everyone else seems to use 100 ohm lines?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dominic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 10:05:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-line-impedance/m-p/576333#M88037</guid>
      <dc:creator>dominicmusgrove</dc:creator>
      <dc:date>2016-07-15T10:05:45Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe line impedance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-line-impedance/m-p/576334#M88038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dominic&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;differential impedance is 85ohm in PCIe gen2 according to&lt;/P&gt;&lt;P&gt;PCIe specification in PCI-SIG.&lt;/P&gt;&lt;P&gt;Also one can references to it, like IDT AN808 or others.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 11:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-line-impedance/m-p/576334#M88038</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-15T11:20:49Z</dc:date>
    </item>
  </channel>
</rss>