<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックu-boot internal code size overflow</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-internal-code-size-overflow/m-p/186159#M8779</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On my mx53_loco board i have a problem:&lt;BR /&gt;when i add the command line help define (CONFIG_SYS_LONGHELP) in the board specific header, building complete successful but when i boot the board i find a corrupted environment (all commmands are unrecognized).&lt;/P&gt;&lt;P&gt;I have this problem even if i increase the size of the CONFIG_EXTRA_ENV_SETTINGS define.&lt;/P&gt;&lt;P&gt;So it seems to be a problem related to size of the u-boot code that overflows somewhere. (memory map re-definition?)&lt;/P&gt;&lt;P&gt;I would to be able to resize internal layout of u-boot correctly...&lt;/P&gt;&lt;P&gt;Can anyone explain me what happens or suggest a helpful link?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Sep 2012 13:12:22 GMT</pubDate>
    <dc:creator>RaffaelePiarull</dc:creator>
    <dc:date>2012-09-05T13:12:22Z</dc:date>
    <item>
      <title>u-boot internal code size overflow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-internal-code-size-overflow/m-p/186159#M8779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On my mx53_loco board i have a problem:&lt;BR /&gt;when i add the command line help define (CONFIG_SYS_LONGHELP) in the board specific header, building complete successful but when i boot the board i find a corrupted environment (all commmands are unrecognized).&lt;/P&gt;&lt;P&gt;I have this problem even if i increase the size of the CONFIG_EXTRA_ENV_SETTINGS define.&lt;/P&gt;&lt;P&gt;So it seems to be a problem related to size of the u-boot code that overflows somewhere. (memory map re-definition?)&lt;/P&gt;&lt;P&gt;I would to be able to resize internal layout of u-boot correctly...&lt;/P&gt;&lt;P&gt;Can anyone explain me what happens or suggest a helpful link?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2012 13:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-internal-code-size-overflow/m-p/186159#M8779</guid>
      <dc:creator>RaffaelePiarull</dc:creator>
      <dc:date>2012-09-05T13:12:22Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot internal code size overflow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-internal-code-size-overflow/m-p/186160#M8780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Raffaele,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In mainline U-boot&amp;nbsp;CONFIG_SYS_LONGHELP is defined in include/configs/mx53loco.h and it works fine there.&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.denx.de/?p=u-boot.git;a=blob;f=include/configs/mx53loco.h;h=8cbaf08e0e1e097ff7856fed028987b9c87db6f8;hb=HEAD" target="_blank"&gt;http://git.denx.de/?p=u-boot.git;a=blob;f=include/configs/mx53loco.h;h=8cbaf08e0e1e097ff7856fed028987b9c87db6f8;hb=HEAD&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I suggest you to use the latest U-boot (from git.denx.de).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2012 23:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-internal-code-size-overflow/m-p/186160#M8780</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2012-09-05T23:10:13Z</dc:date>
    </item>
  </channel>
</rss>