<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX7D  SABRE LCD  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573364#M87757</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The shared community document doesn't seem relevant since it is about E-INK panel that is connected to EPDC expansion port. I've asked about steps for LCD display that is to be connected to LCD connector (J14) present on the other side of i.MX7D SABRE board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Aug 2016 08:20:22 GMT</pubDate>
    <dc:creator>fahad_arslan</dc:creator>
    <dc:date>2016-08-09T08:20:22Z</dc:date>
    <item>
      <title>i.MX7D  SABRE LCD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573362#M87755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What steps (kernel configuration/patches etc.) are required to use LCD with i.MX7D SABRE board?&lt;/P&gt;&lt;P&gt;And whether specific LCD(s) are supported or any LCD may be connected with the target board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Fahad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 16:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573362#M87755</guid>
      <dc:creator>fahad_arslan</dc:creator>
      <dc:date>2016-08-05T16:03:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7D  SABRE LCD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573363#M87756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fahad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According with Android Release Notes, the i.MX7Dual SABRE-SD board supports LCD panel, HDMI display and E-Ink display.&lt;/P&gt;&lt;P&gt;You could refer to the following Community document for additional connection details:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328663"&gt;connecting i.MX7D Sabre(MCIMX7SABRE) and E-INK panel(IMXEBOOKDC4)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 20:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573363#M87756</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-08-08T20:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7D  SABRE LCD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573364#M87757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The shared community document doesn't seem relevant since it is about E-INK panel that is connected to EPDC expansion port. I've asked about steps for LCD display that is to be connected to LCD connector (J14) present on the other side of i.MX7D SABRE board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 08:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573364#M87757</guid>
      <dc:creator>fahad_arslan</dc:creator>
      <dc:date>2016-08-09T08:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7D  SABRE LCD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573365#M87758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fahad,&lt;/P&gt;&lt;P&gt;Please, check &lt;STRONG&gt;i.MX Linux® Release Notes, Rev. L4.1.15_1.2.0-ga, 07/2016&lt;/STRONG&gt; inside &lt;STRONG&gt;L4.1.15_1.2.0_LINUX_DOCS&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="158276_158276.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/122083iDD924B96705D2437/image-size/large?v=v2&amp;amp;px=999" role="button" title="158276_158276.png" alt="158276_158276.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1282iD11CECDA99DA2196/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It also has information about what to add on kernel command line to enable display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 19:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7D-SABRE-LCD/m-p/573365#M87758</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-08-10T19:23:11Z</dc:date>
    </item>
  </channel>
</rss>