<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can imx6q android4.4.2 support 5.0Megapixel usb camera? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6q-android4-4-2-support-5-0Megapixel-usb-camera/m-p/573210#M87740</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what input format and framerate do you use? IPU can support up to 240Mhz,&lt;/P&gt;&lt;P&gt;operating frequency of the interface is calculated in the following way:&lt;/P&gt;&lt;P&gt;F = FH * FW * FPS * BI * DF, BI=1.35, DF = data format, defines the number of cycles needed to send a single pixel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jul 2016 08:44:58 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2016-07-21T08:44:58Z</dc:date>
    <item>
      <title>Can imx6q android4.4.2 support 5.0Megapixel usb camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6q-android4-4-2-support-5-0Megapixel-usb-camera/m-p/573209#M87739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can imx6q android4.4.2 support 5.0Megapixel usb camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My environment:&lt;/P&gt;&lt;P&gt;kernel 3.0.35&lt;/P&gt;&lt;P&gt;android 4.4.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I plug in 5.0M usb camera, the system camera app can preview, but when I click capture button, it just generate a image totally white.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, if I tried with a 0.3M usb camera, it works well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the problem? how to use 5M usb camera in my android 4.4.2 with imx6q?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 01:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6q-android4-4-2-support-5-0Megapixel-usb-camera/m-p/573209#M87739</guid>
      <dc:creator>conteczxy</dc:creator>
      <dc:date>2016-07-15T01:31:01Z</dc:date>
    </item>
    <item>
      <title>Re: Can imx6q android4.4.2 support 5.0Megapixel usb camera?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-imx6q-android4-4-2-support-5-0Megapixel-usb-camera/m-p/573210#M87740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what input format and framerate do you use? IPU can support up to 240Mhz,&lt;/P&gt;&lt;P&gt;operating frequency of the interface is calculated in the following way:&lt;/P&gt;&lt;P&gt;F = FH * FW * FPS * BI * DF, BI=1.35, DF = data format, defines the number of cycles needed to send a single pixel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 08:44:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-imx6q-android4-4-2-support-5-0Megapixel-usb-camera/m-p/573210#M87740</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2016-07-21T08:44:58Z</dc:date>
    </item>
  </channel>
</rss>