<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX6 Boot Mode bits in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Boot-Mode-bits/m-p/572831#M87705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that BOOT_MODE[1:0] are external pins of the processor.&lt;/P&gt;&lt;P&gt;You can pull-up or pull-down them to "program" these bits in hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Aug 2016 07:13:11 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-08-09T07:13:11Z</dc:date>
    <item>
      <title>I.MX6 Boot Mode bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Boot-Mode-bits/m-p/572829#M87703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I want to set the BOOT_MODE[1:0] to 00 so that boot from fuses mode gets activated. But I can't seem to find a way to program these bits from the reference manual. Are these bits(BOOT_MODE[1:0]) also a part of efuses or they belong to a register? Please help!! Regards, Rohini&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 14:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Boot-Mode-bits/m-p/572829#M87703</guid>
      <dc:creator>rohininarasipur</dc:creator>
      <dc:date>2016-08-05T14:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 Boot Mode bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Boot-Mode-bits/m-p/572830#M87704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;BOOT_MODE[1:0] can be accessed via BOOT_MODE0 and BOOT_MODE1 pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 08:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Boot-Mode-bits/m-p/572830#M87704</guid>
      <dc:creator>jan_spurek</dc:creator>
      <dc:date>2016-08-08T08:15:36Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 Boot Mode bits</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Boot-Mode-bits/m-p/572831#M87705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that BOOT_MODE[1:0] are external pins of the processor.&lt;/P&gt;&lt;P&gt;You can pull-up or pull-down them to "program" these bits in hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 07:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Boot-Mode-bits/m-p/572831#M87705</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-08-09T07:13:11Z</dc:date>
    </item>
  </channel>
</rss>