<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.mx6 Quad Core intermittent boot issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Quad-Core-intermittent-boot-issue/m-p/572676#M87702</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jois,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are aware of a boot up issues on the MMPF0100 on revisions Pass1.0 through Pass1.2, typically if power is removed from the board and reapplied within ~ 2 minutes. On MMPF0100 revision Pass2.0 this issue was corrected. For more details, see the PMPF0100 ERRATA, Issue #ER19: &lt;A href="http://cache.freescale.com/files/analog/doc/errata/MMPF0100ER.pdf"&gt;http://cache.freescale.com/files/analog/doc/errata/MMPF0100ER.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Just make sure that you have a new revision of the MMPF100 or you would need the workaround mentioned in the errata document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This boot-up issue can also be related to the POR configuration, try to extend the POR to meet the RTC_XTAL stability as mentioned in this community thread: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/382025"&gt;https://community.nxp.com/thread/382025&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Aug 2016 17:55:51 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2016-08-11T17:55:51Z</dc:date>
    <item>
      <title>i.mx6 Quad Core intermittent boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Quad-Core-intermittent-boot-issue/m-p/572675#M87701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp; We have built custom hardware with i.mx6 quad core processor and MMPF0100F0AEP as PMIC.&lt;/P&gt;&lt;P&gt;&amp;nbsp; we have built 500 boards and we are observing the same issue in 100 boards.&lt;/P&gt;&lt;P&gt;&amp;nbsp; We have also done similar trials on our hardware and still the same issue exists.&lt;/P&gt;&lt;P&gt;&amp;nbsp; What is the solutions for this? It is very urgent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Srinidhi jois&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 05:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Quad-Core-intermittent-boot-issue/m-p/572675#M87701</guid>
      <dc:creator>joissrinidhites</dc:creator>
      <dc:date>2016-08-05T05:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Quad Core intermittent boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Quad-Core-intermittent-boot-issue/m-p/572676#M87702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jois,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are aware of a boot up issues on the MMPF0100 on revisions Pass1.0 through Pass1.2, typically if power is removed from the board and reapplied within ~ 2 minutes. On MMPF0100 revision Pass2.0 this issue was corrected. For more details, see the PMPF0100 ERRATA, Issue #ER19: &lt;A href="http://cache.freescale.com/files/analog/doc/errata/MMPF0100ER.pdf"&gt;http://cache.freescale.com/files/analog/doc/errata/MMPF0100ER.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Just make sure that you have a new revision of the MMPF100 or you would need the workaround mentioned in the errata document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This boot-up issue can also be related to the POR configuration, try to extend the POR to meet the RTC_XTAL stability as mentioned in this community thread: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/382025"&gt;https://community.nxp.com/thread/382025&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 17:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Quad-Core-intermittent-boot-issue/m-p/572676#M87702</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2016-08-11T17:55:51Z</dc:date>
    </item>
  </channel>
</rss>