<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic win 7 doesnt recognize imx6sl custom board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/win-7-doesnt-recognize-imx6sl-custom-board/m-p/572312#M87653</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i connected the production board to the PC (win 7) and the device manager displays it as "Unknown device"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if its not recognized as HID device i cannot use the MFG tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it a driver issue or something else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where can i find the imx6sl windows drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jul 2016 10:16:51 GMT</pubDate>
    <dc:creator>shlomiperlman</dc:creator>
    <dc:date>2016-07-14T10:16:51Z</dc:date>
    <item>
      <title>win 7 doesnt recognize imx6sl custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/win-7-doesnt-recognize-imx6sl-custom-board/m-p/572312#M87653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i connected the production board to the PC (win 7) and the device manager displays it as "Unknown device"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if its not recognized as HID device i cannot use the MFG tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it a driver issue or something else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where can i find the imx6sl windows drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 10:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/win-7-doesnt-recognize-imx6sl-custom-board/m-p/572312#M87653</guid>
      <dc:creator>shlomiperlman</dc:creator>
      <dc:date>2016-07-14T10:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: win 7 doesnt recognize imx6sl custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/win-7-doesnt-recognize-imx6sl-custom-board/m-p/572313#M87654</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi shlomi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check boot pins, 24MHz clock and try suggestions on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/318706"&gt;Mfgtool can't connect in windows7&lt;/A&gt; &lt;/P&gt;&lt;P&gt;use latest mfg tools, no need for special driver&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX6_L4.1.15_1.2.0_MFG_TOOL&amp;amp;appType=file2&amp;amp;location=null&amp;amp;DOWNLOAD_ID=null" title="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=IMX6_L4.1.15_1.2.0_MFG_TOOL&amp;amp;appType=file2&amp;amp;location=null&amp;amp;DOWNLOAD_ID=null"&gt;IMX6_L4.1.15_1.2.0_MFG_TOOL&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 11:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/win-7-doesnt-recognize-imx6sl-custom-board/m-p/572313#M87654</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-14T11:03:47Z</dc:date>
    </item>
  </channel>
</rss>