<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic About imx28 HAB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-imx28-HAB/m-p/566564#M87295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According AN4555 PDF file at the page 19 has like below message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first signature will be used with CALL HAB with offset 0x24 showing original&lt;/P&gt;&lt;P&gt;value ‘0’ and second signature used for authenticating linux_prep with JUMP HAB showing a&lt;/P&gt;&lt;P&gt;value of 1 at offset 0x24. We do this by first copying linux_prep, bin to linux_kernel.bin, then&lt;/P&gt;&lt;P&gt;manually modify byte 0x24 to 1 using a hex editor and include linux_kernel.bin in linux_kernel.csf&lt;/P&gt;&lt;P&gt;for signature generation.&lt;/P&gt;&lt;P&gt;cp linux_prep.bin linux_kernel.bin&lt;/P&gt;&lt;P&gt;using a hex editor set byte 0x24 to 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These message what meaning？&amp;nbsp;&amp;nbsp; How can i sure what offset byte is 0x24 and modify to 0?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jun 2016 09:12:52 GMT</pubDate>
    <dc:creator>bruce_chen</dc:creator>
    <dc:date>2016-06-23T09:12:52Z</dc:date>
    <item>
      <title>About imx28 HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-imx28-HAB/m-p/566564#M87295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According AN4555 PDF file at the page 19 has like below message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first signature will be used with CALL HAB with offset 0x24 showing original&lt;/P&gt;&lt;P&gt;value ‘0’ and second signature used for authenticating linux_prep with JUMP HAB showing a&lt;/P&gt;&lt;P&gt;value of 1 at offset 0x24. We do this by first copying linux_prep, bin to linux_kernel.bin, then&lt;/P&gt;&lt;P&gt;manually modify byte 0x24 to 1 using a hex editor and include linux_kernel.bin in linux_kernel.csf&lt;/P&gt;&lt;P&gt;for signature generation.&lt;/P&gt;&lt;P&gt;cp linux_prep.bin linux_kernel.bin&lt;/P&gt;&lt;P&gt;using a hex editor set byte 0x24 to 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These message what meaning？&amp;nbsp;&amp;nbsp; How can i sure what offset byte is 0x24 and modify to 0?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 09:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-imx28-HAB/m-p/566564#M87295</guid>
      <dc:creator>bruce_chen</dc:creator>
      <dc:date>2016-06-23T09:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: About imx28 HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-imx28-HAB/m-p/566565#M87296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi bruce&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;meaning is described in the same part of text:&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;The execution flow can better be understood using Section 4.2,&lt;/P&gt;&lt;P&gt;“Sample boot descriptor file used for Linux kernel image.”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as example on can look at attached linux_ivt.db, from generated imx-bootlets&lt;/P&gt;&lt;P&gt;(prepare bootlets sources (in ltib/RPM/Build):&lt;/P&gt;&lt;P&gt;./ltib -m prep -p boot_stream.spec )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;//----------------------------------------------------------&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Prepare to boot Linux&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //----------------------------------------------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; load linux_prep;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; load ivt (entry = linux_prep:_start) &amp;gt; 0x8000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; hab call 0x8000;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //----------------------------------------------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp; Load ans start Linux kernel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //----------------------------------------------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; load zImage &amp;gt; 0x40008000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; load ivt (entry = linux_prep:_start) &amp;gt; 0x8000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; hab jump 0x8000;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 01:14:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-imx28-HAB/m-p/566565#M87296</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-24T01:14:42Z</dc:date>
    </item>
  </channel>
</rss>