<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX51 Image Rotator performance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-Image-Rotator-performance/m-p/566538#M87293</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nori&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;data is provided for YUV/RGB format, 8 bits/value&lt;/P&gt;&lt;P&gt;as described in sect.42.1.3.3.2 Image Rotator (IRT),&lt;/P&gt;&lt;P&gt;sorry there is no bit per pixel specification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Can I use Image Rotator for&amp;nbsp;1024x768@60Hz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in theory yes, in practice performance may be affected by available&lt;/P&gt;&lt;P&gt;memory bandwidth (depending on application) as IRT uses&lt;/P&gt;&lt;P&gt;input/output from/to system memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Aug 2016 09:09:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-08-30T09:09:37Z</dc:date>
    <item>
      <title>i.MX51 Image Rotator performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-Image-Rotator-performance/m-p/566537#M87292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Champs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX51 RM, there is this description,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2805i52BEEF22D28846E6/image-size/large?v=v2&amp;amp;px=999" title="imx51_image_rotate.png" alt="imx51_image_rotate.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a LCD with 1024x768@60Hz, the pixel clock is 65MHz.&lt;/P&gt;&lt;P&gt;Simply, 1024x768x60 = 47MHz pixels/sec, which is within the spec 50 M pixels/sec.&lt;/P&gt;&lt;P&gt;Isn't there bit per pixel specification?&lt;/P&gt;&lt;P&gt;Can I use Image Rotator for 1024x768@60Hz?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;BR,&lt;BR /&gt;Nori Shinozaki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 09:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX51-Image-Rotator-performance/m-p/566537#M87292</guid>
      <dc:creator>norishinozaki</dc:creator>
      <dc:date>2016-08-29T09:40:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX51 Image Rotator performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-Image-Rotator-performance/m-p/566538#M87293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nori&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;data is provided for YUV/RGB format, 8 bits/value&lt;/P&gt;&lt;P&gt;as described in sect.42.1.3.3.2 Image Rotator (IRT),&lt;/P&gt;&lt;P&gt;sorry there is no bit per pixel specification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Can I use Image Rotator for&amp;nbsp;1024x768@60Hz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in theory yes, in practice performance may be affected by available&lt;/P&gt;&lt;P&gt;memory bandwidth (depending on application) as IRT uses&lt;/P&gt;&lt;P&gt;input/output from/to system memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 09:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX51-Image-Rotator-performance/m-p/566538#M87293</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-30T09:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX51 Image Rotator performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX51-Image-Rotator-performance/m-p/566539#M87294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;BR, N.S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 09:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX51-Image-Rotator-performance/m-p/566539#M87294</guid>
      <dc:creator>norishinozaki</dc:creator>
      <dc:date>2016-08-30T09:36:40Z</dc:date>
    </item>
  </channel>
</rss>