<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MX28: Using Mfgtool with Mainline kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX28-Using-Mfgtool-with-Mainline-kernel/m-p/565224#M87230</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL 2.6.35 and 3.0.35 (please check attached Linux Manuals USB Chapters)&lt;/P&gt;&lt;P&gt;use ARC USB Driver, while 4.1.15&amp;nbsp; - CHIPIDEA USB Driver, so probably&lt;/P&gt;&lt;P&gt;this may be a reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2016 00:50:27 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-24T00:50:27Z</dc:date>
    <item>
      <title>MX28: Using Mfgtool with Mainline kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX28-Using-Mfgtool-with-Mainline-kernel/m-p/565223#M87229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i want to use a recent Linux kernel as an updater linux for Mfgtool on custom MX28 board. I succeeded to port the FSL_UTP_UPDATER into Kernel 4.2.5, but the performance is bad (FSL 2.6.35 takes 4 minutes and Kernel 4.2.5 takes 11 minutes).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas what could be the reason for this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 16:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX28-Using-Mfgtool-with-Mainline-kernel/m-p/565223#M87229</guid>
      <dc:creator>lategoodbye</dc:creator>
      <dc:date>2016-06-23T16:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: MX28: Using Mfgtool with Mainline kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX28-Using-Mfgtool-with-Mainline-kernel/m-p/565224#M87230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSL 2.6.35 and 3.0.35 (please check attached Linux Manuals USB Chapters)&lt;/P&gt;&lt;P&gt;use ARC USB Driver, while 4.1.15&amp;nbsp; - CHIPIDEA USB Driver, so probably&lt;/P&gt;&lt;P&gt;this may be a reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 00:50:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX28-Using-Mfgtool-with-Mainline-kernel/m-p/565224#M87230</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-24T00:50:27Z</dc:date>
    </item>
    <item>
      <title>Re: MX28: Using Mfgtool with Mainline kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX28-Using-Mfgtool-with-Mainline-kernel/m-p/565225#M87231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved it. It was a combination of multiple issues:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;suboptimal Kernel config&lt;/LI&gt;&lt;LI&gt;wrong version of FSL updater&lt;/LI&gt;&lt;LI&gt;missing DDR support in MMC driver&lt;/LI&gt;&lt;LI&gt;disabled streaming in Chipidea UDC driver&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jul 2016 11:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX28-Using-Mfgtool-with-Mainline-kernel/m-p/565225#M87231</guid>
      <dc:creator>lategoodbye</dc:creator>
      <dc:date>2016-07-03T11:22:08Z</dc:date>
    </item>
  </channel>
</rss>