<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAndroid porting on imx6 solo based custom board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-porting-on-imx6-solo-based-custom-board/m-p/565096#M87224</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi i am trying to port android on my custom board i am using l5 system image and its u image.&lt;/P&gt;&lt;P&gt;my kernel stars and then it try to call init but it gives error .:below is what i am getting.&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p2): using internal journal&lt;BR /&gt;EXT3-fs (mmcblk0p2): recovery complete&lt;BR /&gt;EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode&lt;BR /&gt;VFS: Mounted root (ext3 filesystem) on device 179:2.&lt;BR /&gt;devtmpfs: error mounting -2&lt;BR /&gt;Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)&lt;BR /&gt;Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.&lt;BR /&gt;Rebooting in 5 seconds..&lt;BR /&gt;mxc_restart: Watchdog reset failed to assert reset.&lt;/P&gt;&lt;P&gt;after that nothing happens it dont move forward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 27 Aug 2016 08:26:12 GMT</pubDate>
    <dc:creator>anupamnalgundwa</dc:creator>
    <dc:date>2016-08-27T08:26:12Z</dc:date>
    <item>
      <title>Android porting on imx6 solo based custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-porting-on-imx6-solo-based-custom-board/m-p/565096#M87224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi i am trying to port android on my custom board i am using l5 system image and its u image.&lt;/P&gt;&lt;P&gt;my kernel stars and then it try to call init but it gives error .:below is what i am getting.&lt;/P&gt;&lt;P&gt;EXT3-fs (mmcblk0p2): using internal journal&lt;BR /&gt;EXT3-fs (mmcblk0p2): recovery complete&lt;BR /&gt;EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode&lt;BR /&gt;VFS: Mounted root (ext3 filesystem) on device 179:2.&lt;BR /&gt;devtmpfs: error mounting -2&lt;BR /&gt;Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)&lt;BR /&gt;Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.&lt;BR /&gt;Rebooting in 5 seconds..&lt;BR /&gt;mxc_restart: Watchdog reset failed to assert reset.&lt;/P&gt;&lt;P&gt;after that nothing happens it dont move forward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Aug 2016 08:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-porting-on-imx6-solo-based-custom-board/m-p/565096#M87224</guid>
      <dc:creator>anupamnalgundwa</dc:creator>
      <dc:date>2016-08-27T08:26:12Z</dc:date>
    </item>
  </channel>
</rss>