<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Use of CAAM module for bare metal application in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Use-of-CAAM-module-for-bare-metal-application/m-p/564329#M87165</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your reply. Yes, I could find the simple test which you mention. Like you said, the example is just to create some key blobs and to encrypt/decrypt data. Unfortunately, the example is not using a hash algorithm like the SHA. There exists no example for using it in a bare-metal application?&lt;/P&gt;&lt;P&gt;At least it would help me to get a sequence for the job descriptor to calculate a hash value with the SHA256. Is it possible to stream the input data for the hash calculation for example via a FIFO which is not filled at all at the start of the calculation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jul 2016 06:49:04 GMT</pubDate>
    <dc:creator>srouser526</dc:creator>
    <dc:date>2016-07-13T06:49:04Z</dc:date>
    <item>
      <title>Use of CAAM module for bare metal application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-of-CAAM-module-for-bare-metal-application/m-p/564327#M87163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question. Is it possible to use the CAAM hardware cryptographic functions in a bare-metal application. Are there any drivers provided? I only know, that there exist drivers for linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Especially I like to know of it is possible, to calculate the SHA256 value for any input data in a bare-metal application.&lt;/P&gt;&lt;P&gt;HAB is not providing the simple calculation of a HASH value, isn't it? There are only some abstract functions to authentificate complete image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If there exist a possibility or a driver for the hash calculation is there as well a possibility to stream the input data for the hash calculation? In the best case I like to call a function several times to stream some input data to the CAAM hash module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 15:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-of-CAAM-module-for-bare-metal-application/m-p/564327#M87163</guid>
      <dc:creator>srouser526</dc:creator>
      <dc:date>2016-07-12T15:32:51Z</dc:date>
    </item>
    <item>
      <title>Re: Use of CAAM module for bare metal application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-of-CAAM-module-for-bare-metal-application/m-p/564328#M87164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; stefanrombach&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sdk had some simple tests: caam_blob_gen.c,caam_test.c,&lt;/P&gt;&lt;P&gt;however it was removed from web. For obtaining it please create&lt;/P&gt;&lt;P&gt;service request.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2016 00:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-of-CAAM-module-for-bare-metal-application/m-p/564328#M87164</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-13T00:22:24Z</dc:date>
    </item>
    <item>
      <title>Re: Use of CAAM module for bare metal application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-of-CAAM-module-for-bare-metal-application/m-p/564329#M87165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your reply. Yes, I could find the simple test which you mention. Like you said, the example is just to create some key blobs and to encrypt/decrypt data. Unfortunately, the example is not using a hash algorithm like the SHA. There exists no example for using it in a bare-metal application?&lt;/P&gt;&lt;P&gt;At least it would help me to get a sequence for the job descriptor to calculate a hash value with the SHA256. Is it possible to stream the input data for the hash calculation for example via a FIFO which is not filled at all at the start of the calculation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2016 06:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-of-CAAM-module-for-bare-metal-application/m-p/564329#M87165</guid>
      <dc:creator>srouser526</dc:creator>
      <dc:date>2016-07-13T06:49:04Z</dc:date>
    </item>
  </channel>
</rss>