<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: PING Problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560948#M86951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor, probably I have to add some "code" to "device tree blob"?&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2016 06:38:32 GMT</pubDate>
    <dc:creator>alexlevandovski</dc:creator>
    <dc:date>2016-06-24T06:38:32Z</dc:date>
    <item>
      <title>PING Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560945#M86948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have Board with LAN7500 connected to USB2 iMX6(Freescale). This Board is under Linux 3.10.17 Kernel. As I boot the Board and connect LAN7500 EthernetConnector to Ethernet Cable I see green LED and orange LED are on.Then make LAN7500 UP, check LINK, Ping 172.20.20.20 over eth1(LAN7500). 100% Packet loss. Can you help me in this problem?&lt;/P&gt;&lt;P&gt;Regards Alex&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# ip link set dev eth1 up&lt;/P&gt;&lt;P&gt;IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready&lt;/P&gt;&lt;P&gt;smsc75xx 2-1.2:1.0 eth1: link up, 1000Mbps, full-duplex, lpa 0xC1E1&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# ip link&lt;/P&gt;&lt;P&gt;1: lo: &amp;lt;LOOPBACK,UP,LOWER_UP&amp;gt; mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00&lt;/P&gt;&lt;P&gt;2: can0: &amp;lt;NOARP,ECHO&amp;gt; mtu 16 qdisc noop state DOWN mode DEFAULT qlen 10&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; link/can&lt;/P&gt;&lt;P&gt;3: can1: &amp;lt;NOARP,ECHO&amp;gt; mtu 16 qdisc noop state DOWN mode DEFAULT qlen 10&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; link/can&lt;/P&gt;&lt;P&gt;4: eth0: &amp;lt;NO-CARRIER,BROADCAST,MULTICAST,UP&amp;gt; mtu 1500 qdisc pfifo_fast state DOWN mode DEFAULT qlen 1000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; link/ether 0a:64:5b:0a:b1:73 brd ff:ff:ff:ff:ff:ff&lt;/P&gt;&lt;P&gt;5: eth1: &amp;lt;BROADCAST,MULTICAST,UP,LOWER_UP&amp;gt; mtu 1500 qdisc pfifo_fast state UP mode DEFAULT qlen 1000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; link/ether b6:49:c4:9f:c6:6b brd ff:ff:ff:ff:ff:ff&lt;/P&gt;&lt;P&gt;6: sit0: &amp;lt;NOARP&amp;gt; mtu 1480 qdisc noop state DOWN mode DEFAULT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; link/sit 0.0.0.0 brd 0.0.0.0&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# ping -I eth1 172.20.20.20&lt;/P&gt;&lt;P&gt;PING 172.20.20.20 (172.20.20.20): 56 data bytes&lt;/P&gt;&lt;P&gt;^C&lt;/P&gt;&lt;P&gt;--- 172.20.20.20 ping statistics ---&lt;/P&gt;&lt;P&gt;8 packets transmitted, 0 packets received, 100% packet loss&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~#&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 10:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560945#M86948</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-06-22T10:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: PING Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560946#M86949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to use more new kernel&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fgit.freescale.com%2Fgit%2Fcgit.cgi%2Fimx%2Flinux-2.6-imx.git%2F%3Fh%3Dimx_4.1.15_1.0.0_ga" rel="nofollow" target="_blank"&gt;http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/?h=imx_4.1.15_1.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and use ethtool for debugging, try loopback&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.armadeus.org/wiki/index.php?title=USB_to_Ethernet_adapter" title="http://www.armadeus.org/wiki/index.php?title=USB_to_Ethernet_adapter"&gt;USB to Ethernet adapter - ArmadeusWiki&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 00:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560946#M86949</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-23T00:50:39Z</dc:date>
    </item>
    <item>
      <title>Re: PING Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560947#M86950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor.&lt;/P&gt;&lt;P&gt;Thanks. I'll try it.&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 06:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560947#M86950</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-06-23T06:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: PING Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560948#M86951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor, probably I have to add some "code" to "device tree blob"?&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 06:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560948#M86951</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-06-24T06:38:32Z</dc:date>
    </item>
    <item>
      <title>Re: PING Problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560949#M86952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor, new(last) information. &lt;/P&gt;&lt;P&gt;1. I connected Ethernet cable to imx6 Ethernet Input and after this boot the Board.&lt;/P&gt;&lt;P&gt;2. Then I aktivated LAN7500&amp;nbsp; with&amp;nbsp; ifconfig eth1 up&lt;/P&gt;&lt;P&gt;3.Then I reconnect Ethernet cable from imx6 Ethernet to LAN7500 Ethernet.&lt;/P&gt;&lt;P&gt;4. Then I make ping&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ping -I eth1 172.20.20.20&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; and it was OK.&lt;/P&gt;&lt;P&gt;I think, that some configuration was needed to functionality of LAN7500(IP?). And this configuration made Kernel boot procedure imx6 in Point 1.&lt;/P&gt;&lt;P&gt;LAN7500 used this configuration. Can you help me to explain how can I make this configuration in kernel boot procedure, so that LAN7500 come in UP state after boot Kernel without user aktivity(automatic). And what have to be configured?&lt;/P&gt;&lt;P&gt;thanks in advance.&lt;/P&gt;&lt;P&gt;alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 10:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PING-Problem/m-p/560949#M86952</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-06-24T10:33:57Z</dc:date>
    </item>
  </channel>
</rss>