<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problems while using Mfg tool to write image to imx6ul custom board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-while-using-Mfg-tool-to-write-image-to-imx6ul-custom/m-p/560831#M86933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The firmware of mfgtool is a small linux system that can run on your board, then using the linux commands(in ucl2.xml script)&amp;nbsp; to program the images to your board. So, you can simply change the DCD header (if you are using different DDR) and IOMUX setting that different from the EVK. You can close/disable some drivers and modules that not used during the mfgtool operation. So you don't need to spend time to debug the firmware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Aug 2016 03:30:26 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2016-08-30T03:30:26Z</dc:date>
    <item>
      <title>Problems while using Mfg tool to write image to imx6ul custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-while-using-Mfg-tool-to-write-image-to-imx6ul-custom/m-p/560830#M86932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to write image to emmc of custom board based on imx6ul evk using Mfg tool. I am struck at Jumping to OS image step. Following is the log shown on serial console while using Mfg tool :--&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;U-Boot 2015.04-imx_v2015.04_4.1.15_1.0.0_ga+gd7d7c43 (Aug 25 2016 - 14:54:28)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CPU: Freescale i.MX6UL rev1.0 at 396 MHz&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: Temperature 38 C&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reset cause: POR&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Board: MX6UL 14X14 LPDDR2 ARM2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;I2C: ready&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 256 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;force_idle_bus: sda=0 scl=1 sda.gp=0x3 scl.gp=0x2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;force_idle_bus: failed to clear bus, sda=0 scl=1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;*** Warning - bad CRC, using default environment&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;unsupported panel TFT43AB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;switch to partitions #0, OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc1(part 0) is current device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Net: Ethernet@0x20b4000 is fused, disable it&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;FEC1 MXC: board_eth_init:failed&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;No ethernet found.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Boot from USB for mfgtools&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Use default environment for mfgtools&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Hit any key to stop autoboot: 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x60cc90 ]&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;## Loading init Ramdisk from Legacy Image at 83800000 ...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Image Name: fsl-image-mfgtool-initramfs-imx6&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Image Type: ARM Linux RAMDisk Image (gzip compressed)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Data Size: 7565342 Bytes = 7.2 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Load Address: 00000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Entry Point: 00000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Verifying Checksum ... OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;## Flattened Device Tree blob at 83000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Booting using the fdt blob at 0x83000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Using Device Tree in place at 83000000, end 8300b885&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/tsc@02040000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/sim@0218c000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/sim@021b4000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/can@02090000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/can@02094000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/lcdif@021c8000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/pxp@021cc000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/csi@021c4000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/ethernet@020b4000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/caam@2140000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/usb@02184200:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/spba-bus@02000000/sai@0202c000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/spba-bus@02000000/sai@02030000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/bee@02044000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/serial@021f4000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/serial@021fc000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/spba-bus@02000000/serial@02018000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/spba-bus@02000000/serial@02024000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/pwm@020f0000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/pwm@020f4000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/pwm@020f8000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/pwm@020fc000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02010000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02014000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/i2c@021a8000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02100000/i2c@021f8000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/gpt@020e8000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Modify /soc/aips-bus@02000000/epit@020d4000:status disabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ft_system_setup for mx6&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Starting kernel ...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Booting Linux on physical CPU 0x0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Linux version 4.1.15-1.1.1+gd5d7c02 (pratyush@pratyushGeotech) (gcc version 5.2. 0 (GCC) ) #41 SMP PREEMPT Sat Aug 20 18:09:31 IST 2016&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Reserved memory: failed to allocate memory for node 'linux,cma'&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Memory policy: Data cache writealloc&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PERCPU: Embedded 12 pages/cpu @8fdd3000 s16960 r8192 d24000 u49152&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall =0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mas s_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerial Number= clk_ignore_unused&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PID hash table entries: 1024 (order: 0, 4096 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Memory: 240204K/262144K available (7944K kernel code, 426K rwdata, 2820K rodata, 424K init, 440K bss, 21940K reserved, 0K cma-reserved, 0K highmem)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Virtual kernel memory layout:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; fixmap : 0xffc00000 - 0xfff00000 (3072 kB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; vmalloc : 0x90800000 - 0xff000000 (1768 MB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; lowmem : 0x80000000 - 0x90000000 ( 256 MB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; .text : 0x80008000 - 0x80a8b3a0 (10765 kB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; .init : 0x80a8c000 - 0x80af6000 ( 424 kB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; .data : 0x80af6000 - 0x80b60b00 ( 427 kB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; .bss : 0x80b63000 - 0x80bd1280 ( 441 kB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Preemptible hierarchical RCU implementation.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; Additional per-CPU info printed with stalls.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NR_IRQS:16 nr_irqs:16 16&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mxc_clocksource_init 24000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Switching to timer-based delay loop, resolution 41ns&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79 635851949 ns&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Console: colour dummy device 80x30&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;pid_max: default: 32768 minimum: 301&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: Testing write buffer coherency: ok&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;/cpus/cpu@0 missing clock-frequency property&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU0: thread -1, cpu 0, socket 0, mpidr 80000000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Setting up static identity map for 0x80008280 - 0x800082d8&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Brought up 1 CPUs&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SMP: Total of 1 processors activated (48.00 BogoMIPS).&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CPU: All CPU(s) started in SVC mode.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;devtmpfs: initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112 604462750000 ns&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;pinctrl core: initialized pinctrl subsystem&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 16&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DMA: preallocated 256 KiB pool for atomic coherent allocations&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;cpuidle: using governor ladder&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;cpuidle: using governor menu&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;hw-breakpoint: maximum watchpoint size is 8 bytes.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mxs-dma 1804000.dma-apbh: initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;SCSI subsystem initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver usbfs&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver hub&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new device driver usb&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;i2c i2c-0: IMX I2C adapter registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;i2c i2c-0: can't use DMA&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;i2c i2c-1: IMX I2C adapter registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;i2c i2c-1: can't use DMA&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Linux video capture interface: v2.00&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;pps_core: LinuxPPS API ver. 1 registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;giometti@l inux.it&amp;gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PTP clock support registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MIPI CSI2 driver module loaded&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Advanced Linux Sound Architecture Driver Initialized.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: Core ver 2.20&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 31&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HCI device and connection manager initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HCI socket layer initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: L2CAP socket layer initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: SCO socket layer initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Switched to clocksource mxc_timer1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TCP established hash table entries: 2048 (order: 1, 8192 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TCP bind hash table entries: 2048 (order: 2, 16384 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TCP: Hash tables configured (established 2048 bind 2048)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;UDP hash table entries: 256 (order: 1, 8192 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RPC: Registered named UNIX socket transport module.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RPC: Registered udp transport module.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RPC: Registered tcp transport module.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Trying to unpack rootfs image as initramfs...&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Freeing initrd memory: 7392K (83800000 - 83f38000)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx rpmsg driver is registered.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bus freq driver module loaded&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;futex hash table entries: 256 (order: 2, 16384 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VFS: Disk quotas dquot_6.6.0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NFS: Registering the id_resolver key type&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Key type id_resolver registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Key type id_legacy registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fuse init (API version 7.23)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;io scheduler noop registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;io scheduler deadline registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;io scheduler cfq registered (default)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx-weim 21b8000.weim: Driver registered.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;backlight supply power not found, using dummy regulator&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MIPI DSI driver module loaded&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MIPI DSI driver module loaded&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx-sdma 20ec000.sdma: no event needs to be remapped&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx-sdma 20ec000.sdma: loaded firmware 3.3&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx-sdma 20ec000.sdma: initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a I MX&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;console [ttymxc0] enabled&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 218, base_baud = 5000000) is a IMX&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx sema4 driver is registered.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[drm] Initialized drm 1.1.0 20060810&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[drm] Initialized vivante 1.0.0 20120216 on minor 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;brd: module loaded&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;loop: module loaded&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;spi_gpio spi4: gpio-miso property not found, switching to no-rx mode&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;CAN device driver interface&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;2188000.ethernet supply phy not found, using dummy regulator&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;pps pps0: new PPS source ptp0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC addr ess: d2:f6:2f:ba:e2:d6&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;libphy: fec_enet_mii_bus: probed&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fec 2188000.ethernet eth0: registered PHC device 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ehci-mxc: Freescale On-Chip EHCI Host driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver usb-storage&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver usb_ehset_test&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;2184800.usbmisc supply vbus-wakeup not found, using dummy regulator&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;2184000.usb supply vbus not found, using dummy regulator&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mousedev: PS/2 mouse device common for all mice&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc 000.snvs/20cc000.snvs:snvs-powerkey/input/input0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;read sensor who am i (0xfffffffb)error !&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fxls8471: probe of 0-001e failed with error -22&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as r tc0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;i2c /dev entries driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR NEC protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR RC5(x/sz) protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR RC6 protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR JVC protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR Sony protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR SANYO protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR Sharp protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR MCE Keyboard/mouse protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;IR XMP protocol handler initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;pxp-v4l2 pxp_v4l2: initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;0-000e supply vdd not found, using dummy regulator&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;0-000e supply vddio not found, using dummy regulator&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mag3110 0-000e: check mag3110 chip ID&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mag3110 0-000e: read chip ID 0xfffffffb is not equal to 0xc4!&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mag3110: probe of 0-000e failed with error -22&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx2-wdt 20bc000.wdog: use WDOG_B to reboot.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HCI UART driver ver 2.3&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HCI UART protocol H4 registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HCI UART protocol BCSP registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HCI UART protocol ATH3K registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver bcm203x&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver btusb&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver ath3k&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sdhci: Copyright(c) Pierre Ossman&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;snvs-secvio 20cc000.caam-snvs: can't get snvs clock&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbcore: registered new interface driver usbhid&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;usbhid: USB HID core driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;wm8960 1-001a: Failed to issue reset&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;wm8960: probe of 1-001a failed with error -5&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;fsl-asrc 2034000.asrc: driver registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx-wm8960 sound: failed to find SAI platform device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;imx-wm8960: probe of sound failed with error -22&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc1: MAN_BKOPS_EN bit is not set&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 26&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 10&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sit: IPv6 over IPv4 tunneling driver&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 17&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;can: controller area network core (rev 20120528 abi 9)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;NET: Registered protocol family 29&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;can: raw protocol (rev 20120528)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;can: broadcast manager protocol (rev 20120528 t)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;can: netlink gateway (rev 20130117) max_hops=1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc1: new DDR MMC card at address 0001&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: RFCOMM TTY layer initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: RFCOMM socket layer initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: RFCOMM ver 1.11&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1: mmc1:0001 Q2J54A 3.58 GiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1boot0: mmc1:0001 Q2J54A partition 1 16.0 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1boot1: mmc1:0001 Q2J54A partition 2 16.0 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: BNEP filters: protocol multicast&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1rpmb: mmc1:0001 Q2J54A partition 3 512 KiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: BNEP socket layer initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Bluetooth: HIDP socket layer initialized&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;8021q: 802.1Q VLAN Support v1.8&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Key type dns_resolver registered&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Failed to disable 696MHz OPP&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had made changes to uboot and generated new uboot.imx file for my custom board. Can anyone help out I may be making mistake? Also in imx6ul evk board mfg tool loads zImage at&amp;nbsp;0x80800000, dtb at&amp;nbsp;0x83000000. Hence, for my custom board also will it load at same location or they should be loaded at different address ? If yes that they should be loaded at different address then how should I determine those addresses?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We made few changes and moved a little forward. The serial console shows following messages at the end&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;mmc1: new DDR MMC card at address 0001&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1: mmc1:0001 Q2J54A 3.58 GiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1boot0: mmc1:0001 Q2J54A partition 1 16.0 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1boot1: mmc1:0001 Q2J54A partition 2 16.0 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmcblk1rpmb: mmc1:0001 Q2J54A partition 3 512 KiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;VSD_3V3: disabling&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;can-3v3: disabling&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;clk: Not disabling unused clocks&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ALSA device list:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; No soundcards found.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Freeing unused kernel memory: 388K (8091b000 - 8097c000)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Failed to execute /init (error -13)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sh: cannot set terminal process group (-1): Inappropriate ioctl for device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sh: no job control in this shell&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;sh-4.3# g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While Mfg tool shows message "No device connected" and nothing happens after that with no error messages.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 10:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-while-using-Mfg-tool-to-write-image-to-imx6ul-custom/m-p/560830#M86932</guid>
      <dc:creator>pratyushtomar</dc:creator>
      <dc:date>2016-08-25T10:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: Problems while using Mfg tool to write image to imx6ul custom board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-while-using-Mfg-tool-to-write-image-to-imx6ul-custom/m-p/560831#M86933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The firmware of mfgtool is a small linux system that can run on your board, then using the linux commands(in ucl2.xml script)&amp;nbsp; to program the images to your board. So, you can simply change the DCD header (if you are using different DDR) and IOMUX setting that different from the EVK. You can close/disable some drivers and modules that not used during the mfgtool operation. So you don't need to spend time to debug the firmware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 03:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-while-using-Mfg-tool-to-write-image-to-imx6ul-custom/m-p/560831#M86933</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2016-08-30T03:30:26Z</dc:date>
    </item>
  </channel>
</rss>