<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6ul from qspi-flash boot firmware need to use qspi a? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-from-qspi-flash-boot-firmware-need-to-use-qspi-a/m-p/560535#M86915</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I saw the passage from the imx6ul manual (IMX6ULRM.pdf section 8.6.3)&lt;/P&gt;&lt;P&gt;“The QuadSPI Configuration Parameters Table is built in boot image at fixed offset 0x400 from QSPI NOR A1 base address (368 bytes).”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Does that means qspi-flash boot need qspi a? Could i only use the qspi b ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jul 2016 03:33:52 GMT</pubDate>
    <dc:creator>shauew</dc:creator>
    <dc:date>2016-07-12T03:33:52Z</dc:date>
    <item>
      <title>imx6ul from qspi-flash boot firmware need to use qspi a?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-from-qspi-flash-boot-firmware-need-to-use-qspi-a/m-p/560535#M86915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I saw the passage from the imx6ul manual (IMX6ULRM.pdf section 8.6.3)&lt;/P&gt;&lt;P&gt;“The QuadSPI Configuration Parameters Table is built in boot image at fixed offset 0x400 from QSPI NOR A1 base address (368 bytes).”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Does that means qspi-flash boot need qspi a? Could i only use the qspi b ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 03:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-from-qspi-flash-boot-firmware-need-to-use-qspi-a/m-p/560535#M86915</guid>
      <dc:creator>shauew</dc:creator>
      <dc:date>2016-07-12T03:33:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ul from qspi-flash boot firmware need to use qspi a?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-from-qspi-flash-boot-firmware-need-to-use-qspi-a/m-p/560536#M86916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;port a is always available, port b is configurable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36459i2B8B76F3042EC235/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 06:20:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-from-qspi-flash-boot-firmware-need-to-use-qspi-a/m-p/560536#M86916</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-12T06:20:14Z</dc:date>
    </item>
  </channel>
</rss>