<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 freescale linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/freescale-linux/m-p/560268#M86904</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello guys,&lt;/P&gt;&lt;P&gt;i am trying to work on imx31 series for ma project. can anyone say which linux os is compatible with imx31 family? and how can i get it? and also is all the linux versions compatible with all imx31 series?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jul 2016 11:27:28 GMT</pubDate>
    <dc:creator>sreevidyam</dc:creator>
    <dc:date>2016-07-12T11:27:28Z</dc:date>
    <item>
      <title>freescale linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/freescale-linux/m-p/560268#M86904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello guys,&lt;/P&gt;&lt;P&gt;i am trying to work on imx31 series for ma project. can anyone say which linux os is compatible with imx31 family? and how can i get it? and also is all the linux versions compatible with all imx31 series?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 11:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/freescale-linux/m-p/560268#M86904</guid>
      <dc:creator>sreevidyam</dc:creator>
      <dc:date>2016-07-12T11:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: freescale linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/freescale-linux/m-p/560269#M86905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The i.MX31 is now a legacy product and the available Linux BSP is with the kernel 2.6 on LTIB. You could also check if Timesys provides additional BSP releases at the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://linuxlink.timesys.com/dev_center/imx31" title="https://linuxlink.timesys.com/dev_center/imx31"&gt;https://linuxlink.timesys.com/dev_center/imx31&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If you are start developing, it would be an option considering a newer i.MX processor, like the i.MX6 or i.MX7, which include BPSs with Linux 4.1.15 on the Yocto Project, and also Android 6.0 support:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/imx" title="http://www.nxp.com/imx"&gt;i.MX Applications Processors|ARM® Cores|NXP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2016 20:28:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/freescale-linux/m-p/560269#M86905</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-07-13T20:28:06Z</dc:date>
    </item>
  </channel>
</rss>