<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Compile Problem (L3.0.35_4.1.0 on Ubuntu 14.04 64bit OS) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Compile-Problem-L3-0-35-4-1-0-on-Ubuntu-14-04-64bit-OS/m-p/559534#M86870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dav Jo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If at all possible I would recommend reverting switching to the exact Ubuntu version of the document you’re referring to (&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-98911"&gt;https://community.nxp.com/docs/DOC-98911&lt;/A&gt;) since LTIB is very sensitive to packet versions. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you look at the documentation that is bundled with the L3.0.35_4.1.0 LTIB latest supported Ubuntu version for the host was 9.0.4 which is not too old for most to use. Most community users were able to adapt it to work on Ubuntu 11.04 and there are also some Community Documents for Ubuntu 12.04 (&lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="93454" data-objecttype="102" href="https://community.nxp.com/docs/DOC-93454"&gt;https://community.nxp.com/docs/DOC-93454&lt;/A&gt;&lt;SPAN&gt;) but unfortunately nothing yet for Ubuntu 14.04.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jul 2016 17:27:38 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-07-12T17:27:38Z</dc:date>
    <item>
      <title>Compile Problem (L3.0.35_4.1.0 on Ubuntu 14.04 64bit OS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compile-Problem-L3-0-35-4-1-0-on-Ubuntu-14-04-64bit-OS/m-p/559533#M86869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi. I am using VMware for Ubuntu-14.04.3-desktop-amd64.iso&lt;/P&gt;&lt;P&gt;and I install L3.0.35_4.1.0_130816_source.tar.gz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to patch and refer to &lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="98911" data-objecttype="102" href="https://community.nxp.com/docs/DOC-98911" style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #017bba;"&gt;Compile L3.0.35_4.1.0 on Ubuntu 13.10 64bit OS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But When i write &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;$ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;There are Errors about patch Fail.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Help me Please&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;----------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kyg@ubuntu:~/ltib$ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS.patch&lt;/P&gt;&lt;P&gt;0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS.patch:106: trailing whitespace.&lt;/P&gt;&lt;P&gt;%patch1 -p1 &lt;/P&gt;&lt;P&gt;0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS.patch:144: trailing whitespace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS.patch:164: trailing whitespace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS.patch:166: trailing whitespace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_14.04_64bit_OS.patch:169: trailing whitespace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;error: patch failed: bin/Ltibutils.pm:359&lt;/P&gt;&lt;P&gt;error: bin/Ltibutils.pm: patch does not apply&lt;/P&gt;&lt;P&gt;error: patch failed: dist/lfs-5.1/base_libs/base_libs.spec:296&lt;/P&gt;&lt;P&gt;error: dist/lfs-5.1/base_libs/base_libs.spec: patch does not apply&lt;/P&gt;&lt;P&gt;error: patch failed: dist/lfs-5.1/m4/m4.spec:9&lt;/P&gt;&lt;P&gt;error: dist/lfs-5.1/m4/m4.spec: patch does not apply&lt;/P&gt;&lt;P&gt;error: patch failed: dist/lfs-5.1/ncurses/ncurses.spec:31&lt;/P&gt;&lt;P&gt;error: dist/lfs-5.1/ncurses/ncurses.spec: patch does not apply&lt;/P&gt;&lt;P&gt;error: patch failed: dist/lfs-5.1/openssl/openssl.spec:10&lt;/P&gt;&lt;P&gt;error: dist/lfs-5.1/openssl/openssl.spec: patch does not apply&lt;/P&gt;&lt;P&gt;error: patch failed: dist/lfs-5.1/xorg-server/xorg-server.spec:11&lt;/P&gt;&lt;P&gt;error: dist/lfs-5.1/xorg-server/xorg-server.spec: patch does not apply&lt;/P&gt;&lt;P&gt;error: pkgs/m4-1.4.16-1383761043.patch: already exists in working directory&lt;/P&gt;&lt;P&gt;error: pkgs/m4-1.4.16-1383761043.patch.md5: already exists in working directory&lt;/P&gt;&lt;P&gt;error: pkgs/openssl-1.0.1c-1398677566.patch: already exists in working directory&lt;/P&gt;&lt;P&gt;error: pkgs/openssl-1.0.1c-1398677566.patch.md5: already exists in working directory&lt;/P&gt;&lt;P&gt;error: pkgs/xorg-server-1.6.1-1398785267.patch: already exists in working directory&lt;/P&gt;&lt;P&gt;error: pkgs/xorg-server-1.6.1-1398785267.patch.md5: already exists in working directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 02:31:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compile-Problem-L3-0-35-4-1-0-on-Ubuntu-14-04-64bit-OS/m-p/559533#M86869</guid>
      <dc:creator>youngguekim</dc:creator>
      <dc:date>2016-07-12T02:31:14Z</dc:date>
    </item>
    <item>
      <title>Re: Compile Problem (L3.0.35_4.1.0 on Ubuntu 14.04 64bit OS)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compile-Problem-L3-0-35-4-1-0-on-Ubuntu-14-04-64bit-OS/m-p/559534#M86870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dav Jo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If at all possible I would recommend reverting switching to the exact Ubuntu version of the document you’re referring to (&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-98911"&gt;https://community.nxp.com/docs/DOC-98911&lt;/A&gt;) since LTIB is very sensitive to packet versions. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you look at the documentation that is bundled with the L3.0.35_4.1.0 LTIB latest supported Ubuntu version for the host was 9.0.4 which is not too old for most to use. Most community users were able to adapt it to work on Ubuntu 11.04 and there are also some Community Documents for Ubuntu 12.04 (&lt;/SPAN&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="93454" data-objecttype="102" href="https://community.nxp.com/docs/DOC-93454"&gt;https://community.nxp.com/docs/DOC-93454&lt;/A&gt;&lt;SPAN&gt;) but unfortunately nothing yet for Ubuntu 14.04.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 17:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compile-Problem-L3-0-35-4-1-0-on-Ubuntu-14-04-64bit-OS/m-p/559534#M86870</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-07-12T17:27:38Z</dc:date>
    </item>
  </channel>
</rss>