<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: X server for second display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/X-server-for-second-display/m-p/557632#M86690</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply. I have given the same parameters and i got both displays working as i have already told in the previous post. But now my requirement is to have X-server running on both displays which can be made possible by configuring the xorg.conf properly for multiple displays. I need support in this case. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jul 2016 04:24:23 GMT</pubDate>
    <dc:creator>danielchempolay</dc:creator>
    <dc:date>2016-07-13T04:24:23Z</dc:date>
    <item>
      <title>X server for second display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/X-server-for-second-display/m-p/557630#M86688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I had been trying to bring up two displays simultaneously in i.mx6qsabreauto EVK and i was successful in bringing up HDMI and LVDS0 in the same. I could run two frame buffer based applications in both displays simultaneously.&lt;/P&gt;&lt;P&gt;Now, my requirement is to run X11 based applications on the same displays. I have LVDS0 running with X-server succesfully and i'm able to lauch X11 based application in the same whereas i'm unable to lauch X11 based application in HDMI display. &lt;/P&gt;&lt;P&gt;Has any one got a clear idea to run X-server for two displays simultaneously?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jul 2016 06:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/X-server-for-second-display/m-p/557630#M86688</guid>
      <dc:creator>danielchempolay</dc:creator>
      <dc:date>2016-07-11T06:40:42Z</dc:date>
    </item>
    <item>
      <title>Re: X server for second display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/X-server-for-second-display/m-p/557631#M86689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For latest Kernel based 4.1.15 BSP, check the release notes document; as example using primarily display on HDMI with 1080P60 mode and secondarily LVDS with XGA mode, you need edit video=mxcfb0:dev=hdmi, 1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;video=mxcfb1:dev=ldb,if=RGB666 enviroment variable at kernel boot parameters&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 15:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/X-server-for-second-display/m-p/557631#M86689</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2016-07-12T15:54:05Z</dc:date>
    </item>
    <item>
      <title>Re: X server for second display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/X-server-for-second-display/m-p/557632#M86690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply. I have given the same parameters and i got both displays working as i have already told in the previous post. But now my requirement is to have X-server running on both displays which can be made possible by configuring the xorg.conf properly for multiple displays. I need support in this case. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2016 04:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/X-server-for-second-display/m-p/557632#M86690</guid>
      <dc:creator>danielchempolay</dc:creator>
      <dc:date>2016-07-13T04:24:23Z</dc:date>
    </item>
  </channel>
</rss>