<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: No Console for BSP Recipe in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-Console-for-BSP-Recipe/m-p/557374#M86678</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;is there any log message when booting?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jul 2016 08:07:54 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2016-07-12T08:07:54Z</dc:date>
    <item>
      <title>No Console for BSP Recipe</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-Console-for-BSP-Recipe/m-p/557373#M86677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I have generated a new recipe for a custom i.MX6 board based on the Freescale core-image-sato recipe. The recipe is below. When the system boots, I get the four penguins and the Yocto progress bar, but never get the console screen. Any ideas what I am missing that is preventing the console screen from being displayed? Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;New recipe:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DESCRIPTION = "Image with Sato, a mobile environment and visual style for \&lt;/P&gt;&lt;P&gt;mobile devices. The image supports X11 with a Sato theme, Pimlico \&lt;/P&gt;&lt;P&gt;applications, and contains terminal, editor, and file manager."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_FEATURES += "splash x11-base ssh-server-openssh hwcodecs"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LICENSE = "MIT"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;inherit core-image extrausers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PACKAGE_INSTALL += " \&lt;/P&gt;&lt;P&gt;&amp;nbsp; alsa-utils-speakertest \&lt;/P&gt;&lt;P&gt;&amp;nbsp; alsa-utils-aplay \&lt;/P&gt;&lt;P&gt;&amp;nbsp; mplayer2 \&lt;/P&gt;&lt;P&gt;&amp;nbsp; psplash \&lt;/P&gt;&lt;P&gt;&amp;nbsp; xserver-nodm-init \&lt;/P&gt;&lt;P&gt;&amp;nbsp; rsync \&lt;/P&gt;&lt;P&gt;&amp;nbsp; udev-automountconf \&lt;/P&gt;&lt;P&gt;&amp;nbsp; nano \&lt;/P&gt;&lt;P&gt;&amp;nbsp; alsa-state \ &lt;/P&gt;&lt;P&gt;&amp;nbsp; xcursor-transparent-theme \&lt;/P&gt;&lt;P&gt;&amp;nbsp; unzip \&lt;/P&gt;&lt;P&gt;&amp;nbsp; x11vnc \&lt;/P&gt;&lt;P&gt;&amp;nbsp; gpio-setup-c398 \&lt;/P&gt;&lt;P&gt;&amp;nbsp; rs485-config \&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;REQUIRED_DISTRO_FEATURES = "x11"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EXTRA_USERS_PARAMS = "\&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; useradd -P bpguest -d /home/bpguest -s /bin/bash bpguest;" &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jul 2016 15:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-Console-for-BSP-Recipe/m-p/557373#M86677</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2016-07-11T15:40:08Z</dc:date>
    </item>
    <item>
      <title>Re: No Console for BSP Recipe</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-Console-for-BSP-Recipe/m-p/557374#M86678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;is there any log message when booting?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 08:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-Console-for-BSP-Recipe/m-p/557374#M86678</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2016-07-12T08:07:54Z</dc:date>
    </item>
  </channel>
</rss>