<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 LCD 8-bit bus/RGB565 support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LCD-8-bit-bus-RGB565-support/m-p/556414#M86604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if an LCD with an 8-bit bus and RGB565 color space is supported in any i.MX product (preferably i.MX6UL).&lt;/P&gt;&lt;P&gt;A pixel is represented by an 16-bit number on the 8-bit bus, so 2 clocks are needed to drive 1 pixel.&amp;nbsp;An example of such LCD is ili9335.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is supported:&lt;/P&gt;&lt;P&gt;1) how do I wire this&lt;/P&gt;&lt;P&gt;2) how do I load the driver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Yocto as operating system and have the DART-6UL demo board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Aug 2016 14:06:52 GMT</pubDate>
    <dc:creator>jonver</dc:creator>
    <dc:date>2016-08-24T14:06:52Z</dc:date>
    <item>
      <title>LCD 8-bit bus/RGB565 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-8-bit-bus-RGB565-support/m-p/556414#M86604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wonder if an LCD with an 8-bit bus and RGB565 color space is supported in any i.MX product (preferably i.MX6UL).&lt;/P&gt;&lt;P&gt;A pixel is represented by an 16-bit number on the 8-bit bus, so 2 clocks are needed to drive 1 pixel.&amp;nbsp;An example of such LCD is ili9335.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is supported:&lt;/P&gt;&lt;P&gt;1) how do I wire this&lt;/P&gt;&lt;P&gt;2) how do I load the driver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Yocto as operating system and have the DART-6UL demo board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 14:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-8-bit-bus-RGB565-support/m-p/556414#M86604</guid>
      <dc:creator>jonver</dc:creator>
      <dc:date>2016-08-24T14:06:52Z</dc:date>
    </item>
    <item>
      <title>Re: LCD 8-bit bus/RGB565 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-8-bit-bus-RGB565-support/m-p/556415#M86605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems i80 ili9335 could be supported by i.MX6UL according to&lt;/P&gt;&lt;P&gt;Table 32-3. Pin use in MPU Mode and VSYNC Mode i.MX6UL Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX6ULRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;8080 mode driver example&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-95559" title="https://community.freescale.com/docs/DOC-95559"&gt;Patch for i.MX28's 8080 mode Lcd panel driver | NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 23:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-8-bit-bus-RGB565-support/m-p/556415#M86605</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-24T23:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: LCD 8-bit bus/RGB565 support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LCD-8-bit-bus-RGB565-support/m-p/556416#M86606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i80 interface display driver patch is also ready for iMX6UL:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-331754"&gt;https://community.nxp.com/docs/DOC-331754&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 03:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LCD-8-bit-bus-RGB565-support/m-p/556416#M86606</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2016-08-25T03:38:53Z</dc:date>
    </item>
  </channel>
</rss>