<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6 Crash when do GPU stability test in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554390#M86433</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do GPU test on our board, It's base on SABRESD Board.But we change ddr3 to lpddr2. And using 32 bit single channel mode with 2 chip selects, 512B pre channel. We can pass ddr_stress_tester more then 2 hours&amp;nbsp; (ver2.52).&lt;/P&gt;&lt;P&gt;And we also pass classic tset (without gpu) more then 4 hours. But when we test with GPU, the system will hang in&amp;nbsp;5 minutes (always less then 2 minutes), and without any&amp;nbsp;logs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We check&amp;nbsp;all&amp;nbsp;power domains are normally... How do i to verify to debug ? Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;David&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Aug 2016 03:12:06 GMT</pubDate>
    <dc:creator>david5icp</dc:creator>
    <dc:date>2016-08-25T03:12:06Z</dc:date>
    <item>
      <title>IMX6 Crash when do GPU stability test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554390#M86433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do GPU test on our board, It's base on SABRESD Board.But we change ddr3 to lpddr2. And using 32 bit single channel mode with 2 chip selects, 512B pre channel. We can pass ddr_stress_tester more then 2 hours&amp;nbsp; (ver2.52).&lt;/P&gt;&lt;P&gt;And we also pass classic tset (without gpu) more then 4 hours. But when we test with GPU, the system will hang in&amp;nbsp;5 minutes (always less then 2 minutes), and without any&amp;nbsp;logs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We check&amp;nbsp;all&amp;nbsp;power domains are normally... How do i to verify to debug ? Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;&lt;P&gt;David&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 03:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554390#M86433</guid>
      <dc:creator>david5icp</dc:creator>
      <dc:date>2016-08-25T03:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Crash when do GPU stability test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554391#M86434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;crash can be caused by gpu bugs, so may be recommended to use&lt;BR /&gt;latest L4.1.15 were they were fixed. &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Fi.mx-applications-processors%2Fi.mx-6-processors%2Fi.mx6qp%2Fi.mx-6-series-software-and-development-tool-resources%3AIMX6_SW" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW&lt;/A&gt;&lt;BR /&gt;Another cause may be power ripples, note ddr tester does not stress well&lt;BR /&gt;power supplies. For example one can try the following experiments to determine &lt;BR /&gt;if it is a hardware PCB issue. Hand solder 22uF capacitors directly under center of chip. &amp;nbsp;&lt;BR /&gt;Solder on top of the 0402 chips.&lt;BR /&gt;Have software Increase voltages of ARM_CAP, SOC_CAP, PU_CAP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 03:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554391#M86434</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-25T03:30:07Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Crash when do GPU stability test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554392#M86435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks for your reply so quickly... All power domains have more than 22uF on CPU buttom side. And i also adjust ARM_CAP, SOC_CAP, PU_CAP to 1.3v, but still hang. The ripple of these power are less 30mV&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I also do a test, to keep CPU clock rate on 996Mhz and set GPU3D clock rate to 3/64, it will pass the test more than 2 hours.&lt;SPAN&gt;Does it mean&lt;/SPAN&gt; HW issue&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 05:32:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554392#M86435</guid>
      <dc:creator>david5icp</dc:creator>
      <dc:date>2016-08-25T05:32:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Crash when do GPU stability test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554393#M86436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the system completly freeze until the watchdog reset occurs? I assume it's another problem because the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;arbitration within the memory controller?&lt;BR /&gt;LPDDR2 has much less bus bandwith, thus causing problems when the GPU3D gets "too hungry".&lt;BR /&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/935193?commentID=935193#comment-935321" title="https://community.nxp.com/message/935193?commentID=935193#comment-935321"&gt;https://community.nxp.com/message/935193?commentID=935193#comment-935321&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 14:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Crash-when-do-GPU-stability-test/m-p/554393#M86436</guid>
      <dc:creator>michaelguntli</dc:creator>
      <dc:date>2017-08-30T14:19:38Z</dc:date>
    </item>
  </channel>
</rss>