<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: menuconfig in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/menuconfig/m-p/552916#M86337</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Aravinthkumar Jayaprakasam!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would also recommend looking at the following Yocto Tutorial where the kernel is configured outside of bitbake, which is useful in some circunstances.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94196"&gt;Yocto Training - Task #5&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may need to use a different kernel recipe depending on which Release of the BSP or Branch from the FSL Community BSP you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jul 2016 17:12:22 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2016-07-12T17:12:22Z</dc:date>
    <item>
      <title>menuconfig</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/menuconfig/m-p/552914#M86335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to get the menuconfig to enable/disable the required drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will bitbake linux-imx -c menuconfig helps?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jul 2016 12:03:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/menuconfig/m-p/552914#M86335</guid>
      <dc:creator>santhosha</dc:creator>
      <dc:date>2016-07-11T12:03:48Z</dc:date>
    </item>
    <item>
      <title>Re: menuconfig</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/menuconfig/m-p/552915#M86336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/santhosha"&gt;santhosha&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;Run the &lt;CODE class="filename"&gt;menuconfig&lt;/CODE&gt; command:&lt;/P&gt;&lt;P&gt;=&amp;gt; bitbake linux-yocto -c menuconfig&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your Reference:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.yoctoproject.org/docs/1.6.1/kernel-dev/kernel-dev.html" title="http://www.yoctoproject.org/docs/1.6.1/kernel-dev/kernel-dev.html"&gt;Yocto Project Linux Kernel Development Manual&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 05:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/menuconfig/m-p/552915#M86336</guid>
      <dc:creator>aravinthkumarja</dc:creator>
      <dc:date>2016-07-12T05:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: menuconfig</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/menuconfig/m-p/552916#M86337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Aravinthkumar Jayaprakasam!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would also recommend looking at the following Yocto Tutorial where the kernel is configured outside of bitbake, which is useful in some circunstances.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94196"&gt;Yocto Training - Task #5&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may need to use a different kernel recipe depending on which Release of the BSP or Branch from the FSL Community BSP you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 17:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/menuconfig/m-p/552916#M86337</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-07-12T17:12:22Z</dc:date>
    </item>
  </channel>
</rss>