<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6 PCIe EP Cannot configure BAR1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552909#M86330</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With the IMX6 configured as a PCIe endpoint, I try to setup BAR0 and BAR1 as 32 bit memory BARs.&amp;nbsp; The problem is that if BAR0 is configured to be a 32 bit memory BAR it seems that whatever I set in the BAR1 mask register is ignored.&amp;nbsp; This is what I do in the code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;// setup BAR0 and its mask&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;RegWrite(Registers32::PCIE_EP_BAR0, 0x0);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;RegWrite(Registers32::PCIE_EP_MASK0, 0xFFFF);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;// setup BAR1 and its mask&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;RegWrite(Registers32::PCIE_EP_BAR1, 0x0);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;P&gt;RegWrite(Registers32::PCIE_EP_MASK1, 0xFFFF);&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the RC enumerates the endpoint and writes 0xFFFFFFFF to each BAR and then reads them back, BAR0 returns 0xFFFF0000 as expected.&amp;nbsp; But BAR1 returns 0x00000000.&amp;nbsp; If I change BAR0 to be a 64 bit BAR (RegWrite(Registers32::PCIE_EP_BAR0, 0x4);) but change nothing else, then BAR1 seems to work and the RC sees it request 64K of memory as expected. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a PCIe bus analyzer to verify the config reads and writes so I know it's not an issue with the RC.&amp;nbsp; These are the values actually going across the wire to and from the IMX6. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can a freescale engineer look into this please?&amp;nbsp; Both the datasheet and the linux example code do not enable BAR1 as a 32 bit BAR so I'm wondering if this has ever been tested or if there is a bug in the part itself.&amp;nbsp; Thanks. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Jun 2016 23:13:02 GMT</pubDate>
    <dc:creator>elijahbrown</dc:creator>
    <dc:date>2016-06-20T23:13:02Z</dc:date>
    <item>
      <title>IMX6 PCIe EP Cannot configure BAR1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552909#M86330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With the IMX6 configured as a PCIe endpoint, I try to setup BAR0 and BAR1 as 32 bit memory BARs.&amp;nbsp; The problem is that if BAR0 is configured to be a 32 bit memory BAR it seems that whatever I set in the BAR1 mask register is ignored.&amp;nbsp; This is what I do in the code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;// setup BAR0 and its mask&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;RegWrite(Registers32::PCIE_EP_BAR0, 0x0);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;RegWrite(Registers32::PCIE_EP_MASK0, 0xFFFF);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;// setup BAR1 and its mask&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;RegWrite(Registers32::PCIE_EP_BAR1, 0x0);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;P&gt;RegWrite(Registers32::PCIE_EP_MASK1, 0xFFFF);&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the RC enumerates the endpoint and writes 0xFFFFFFFF to each BAR and then reads them back, BAR0 returns 0xFFFF0000 as expected.&amp;nbsp; But BAR1 returns 0x00000000.&amp;nbsp; If I change BAR0 to be a 64 bit BAR (RegWrite(Registers32::PCIE_EP_BAR0, 0x4);) but change nothing else, then BAR1 seems to work and the RC sees it request 64K of memory as expected. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a PCIe bus analyzer to verify the config reads and writes so I know it's not an issue with the RC.&amp;nbsp; These are the values actually going across the wire to and from the IMX6. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can a freescale engineer look into this please?&amp;nbsp; Both the datasheet and the linux example code do not enable BAR1 as a 32 bit BAR so I'm wondering if this has ever been tested or if there is a bug in the part itself.&amp;nbsp; Thanks. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 23:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552909#M86330</guid>
      <dc:creator>elijahbrown</dc:creator>
      <dc:date>2016-06-20T23:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 PCIe EP Cannot configure BAR1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552910#M86331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thought I would also paste the linux demo code provided by freescale as well.&amp;nbsp; Based on these comments and my experience, should we assume there is indeed a hardware issue with using BAR1, BAR3, BAR4 and BAR5?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;/* 32bit none-prefetchable 8M bytes memory on bar0 */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(0x0, dbi_base + PCI_BASE_ADDRESS_0);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(SZ_8M - 1, dbi_base + (1 &amp;lt;&amp;lt; 12) + PCI_BASE_ADDRESS_0);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; /* None used bar1 */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(0x0, dbi_base + PCI_BASE_ADDRESS_1);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(0, dbi_base + (1 &amp;lt;&amp;lt; 12) + PCI_BASE_ADDRESS_1);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; /* 4K bytes IO on bar2 */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(0x1, dbi_base + PCI_BASE_ADDRESS_2);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(SZ_4K - 1, dbi_base + (1 &amp;lt;&amp;lt; 12) + PCI_BASE_ADDRESS_2);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; /*&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;nbsp; * 32bit prefetchable 1M bytes memory on bar3&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;nbsp; * FIXME BAR MASK3 is not changable, the size&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;nbsp; * is fixed to 256 bytes.&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;nbsp; */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(0x8, dbi_base + PCI_BASE_ADDRESS_3);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(SZ_1M - 1, dbi_base + (1 &amp;lt;&amp;lt; 12) + PCI_BASE_ADDRESS_3);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; /*&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;nbsp; * 64bit prefetchable 1M bytes memory on bar4-5.&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;nbsp; * FIXME BAR4,5 are not enabled yet&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;nbsp; */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(0xc, dbi_base + PCI_BASE_ADDRESS_4);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(SZ_1M - 1, dbi_base + (1 &amp;lt;&amp;lt; 12) + PCI_BASE_ADDRESS_4);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt; writel(0, dbi_base + (1 &amp;lt;&amp;lt; 12) + PCI_BASE_ADDRESS_5);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 02:07:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552910#M86331</guid>
      <dc:creator>elijahbrown</dc:creator>
      <dc:date>2016-06-21T02:07:49Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 PCIe EP Cannot configure BAR1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552911#M86332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From R&amp;amp;D:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BAR0 thru 4 are different.&lt;/P&gt;&lt;P&gt;BAR0+BAR1 as 64 bit addressing bar, type memory, prefetchable, mask 0xfffff, mask&lt;/P&gt;&lt;P&gt;writable. So Bar1 can’t be used separately.&lt;/P&gt;&lt;P&gt;BAR2 : 32 bit addressing , type memory, prefetchable , mask 0xfffff, mask writable&lt;/P&gt;&lt;P&gt;BAR3 : 32 bit addressing , type IO, mask 0xff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 09:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552911#M86332</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-06-21T09:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 PCIe EP Cannot configure BAR1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552912#M86333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&amp;nbsp; From the reference manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The core provides three pairs of 32-bit BARs for each implemented function. Each pair&lt;/P&gt;&lt;P&gt;(BARs 0 and 1, BARs 2 and 3, BARs 4 and 5) can be configured as follows:&lt;/P&gt;&lt;P&gt;• One 64-bit BAR: For example, BARs 0 and 1 are combined to form a single 64-bit&lt;/P&gt;&lt;P&gt;BAR.&lt;/P&gt;&lt;P&gt;• Two 32-bit BARs: For example, BARs 0 and 1 are two independent 32-bit BARs.&lt;/P&gt;&lt;P&gt;• One 32-bit BAR: For example, BAR 0 is a 32-bit BAR and BAR 1 is either disabled&lt;/P&gt;&lt;P&gt;or removed from the core altogether to reduce gate count.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the reference manual is incorrect, the hardware is not actually capable of being configured this way?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 18:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552912#M86333</guid>
      <dc:creator>elijahbrown</dc:creator>
      <dc:date>2016-06-21T18:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 PCIe EP Cannot configure BAR1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552913#M86334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; the information from R&amp;amp;D is declared as non-documented feature. &lt;/P&gt;&lt;P&gt;Please let me know if it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 03:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-PCIe-EP-Cannot-configure-BAR1/m-p/552913#M86334</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-06-23T03:58:27Z</dc:date>
    </item>
  </channel>
</rss>