<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 SABRE Board for Smart Devices Linux Boot Fail Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SABRE-Board-for-Smart-Devices-Linux-Boot-Fail-Kernel-panic/m-p/552705#M86310</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mianbo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to prepare card using attached Linux Guide&lt;/P&gt;&lt;P&gt;Chapter 8 Using a Linux Host to Set Up an SD/MMC Card&lt;/P&gt;&lt;P&gt;and check procedure using Demo Images&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=133…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Aug 2016 00:04:43 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-08-25T00:04:43Z</dc:date>
    <item>
      <title>i.MX6 SABRE Board for Smart Devices Linux Boot Fail Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SABRE-Board-for-Smart-Devices-Linux-Boot-Fail-Kernel-panic/m-p/552704#M86309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I burn my uboot image and kernel image ,file system using the "Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER"&lt;/P&gt;&lt;P&gt;but after rebooting from SD,it failed ,the uart output infor is as follows,there is a kernel panic info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2009.08 (Aug 16 2013 - 12:04:20)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6 family TO1.2 at 792 MHz&lt;BR /&gt;Thermal sensor with ratio = 187&lt;BR /&gt;Temperature: 37 C, calibration data 0x5a05017d&lt;BR /&gt;mx6q pll1: 792MHz&lt;BR /&gt;mx6q pll2: 528MHz&lt;BR /&gt;mx6q pll3: 480MHz&lt;BR /&gt;mx6q pll8: 50MHz&lt;BR /&gt;ipg clock : 66000000Hz&lt;BR /&gt;ipg per clock : 66000000Hz&lt;BR /&gt;uart clock : 80000000Hz&lt;BR /&gt;cspi clock : 60000000Hz&lt;BR /&gt;ahb clock : 132000000Hz&lt;BR /&gt;axi clock : 264000000Hz&lt;BR /&gt;emi_slow clock: 132000000Hz&lt;BR /&gt;ddr clock : 528000000Hz&lt;BR /&gt;usdhc1 clock : 198000000Hz&lt;BR /&gt;usdhc2 clock : 198000000Hz&lt;BR /&gt;usdhc3 clock : 198000000Hz&lt;BR /&gt;usdhc4 clock : 198000000Hz&lt;BR /&gt;nfc clock : 24000000Hz&lt;BR /&gt;Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]&lt;BR /&gt;Boot Device: SD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GB&lt;BR /&gt;MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Found PFUZE100! deviceid=10,revid=11&lt;BR /&gt;Net: got MAC address from IIM: 00:04:9f:02:af:f3&lt;BR /&gt;FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;mmc2 is current device&lt;/P&gt;&lt;P&gt;MMC read: dev # 2, block # 2048, count 8192 ... 8192 blocks read: OK&lt;BR /&gt;## Booting kernel from Legacy Image at 10800000 ...&lt;BR /&gt; Image Name: Linux-3.0.15&lt;BR /&gt; Image Type: ARM Linux Kernel Image (uncompressed)&lt;BR /&gt; Data Size: 3355508 Bytes = 3.2 MB&lt;BR /&gt; Load Address: 10008000&lt;BR /&gt; Entry Point: 10008000&lt;BR /&gt; Verifying Checksum ... OK&lt;BR /&gt; Loading Kernel Image ... OK&lt;BR /&gt;OK&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Uncompressing Linux... done, booting the kernel.&lt;BR /&gt;Linux version 3.0.15 (hhj@ubuntu) (gcc version 4.6.3 20120105 (prerelease) (crosstool-NG linaro-1.13.1-2012.01-20120125 - Linaro GCC 2012.01) ) #1 SMP PREEMPT Sat Sep 12 17:13:36 CST 2015&lt;BR /&gt;CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d&lt;BR /&gt;CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Machine: Freescale i.MX 6Quad Sabre-SD Board&lt;BR /&gt;Ignoring unrecognised tag 0x54410008&lt;BR /&gt;Memory policy: ECC disabled, Data cache writealloc&lt;BR /&gt;PERCPU: Embedded 7 pages/cpu @8c008000 s5216 r8192 d15264 u32768&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on. Total pages: 227328&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24&lt;BR /&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Memory: 640MB 256MB = 896MB total&lt;BR /&gt;Memory: 901740k/901740k available, 146836k reserved, 0K highmem&lt;BR /&gt;Virtual kernel memory layout:&lt;BR /&gt; vector : 0xffff0000 - 0xffff1000 ( 4 kB)&lt;BR /&gt; fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)&lt;BR /&gt; DMA : 0xf4600000 - 0xffe00000 ( 184 MB)&lt;BR /&gt; vmalloc : 0xc0800000 - 0xf2000000 ( 792 MB)&lt;BR /&gt; lowmem : 0x80000000 - 0xc0000000 (1024 MB)&lt;BR /&gt; pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)&lt;BR /&gt; modules : 0x7f000000 - 0x7fe00000 ( 14 MB)&lt;BR /&gt; .init : 0x80008000 - 0x80036000 ( 184 kB)&lt;BR /&gt; .text : 0x80036000 - 0x806048b8 (5947 kB)&lt;BR /&gt; .data : 0x80606000 - 0x8064da20 ( 287 kB)&lt;BR /&gt; .bss : 0x8064da44 - 0x80677e6c ( 170 kB)&lt;BR /&gt;SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1&lt;BR /&gt;Preemptible hierarchical RCU implementation.&lt;BR /&gt;NR_IRQS:496&lt;BR /&gt;MXC GPIO hardware&lt;BR /&gt;sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms&lt;BR /&gt;MXC_Early serial console at MMIO 0x2020000 (options '115200')&lt;BR /&gt;bootconsole [ttymxc0] enabled&lt;BR /&gt;Console: colour dummy device 80x30&lt;BR /&gt;Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 512&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available&lt;BR /&gt;CPU1: Booted secondary processor&lt;BR /&gt;CPU2: Booted secondary processor&lt;BR /&gt;CPU3: Booted secondary processor&lt;BR /&gt;Brought up 4 CPUs&lt;BR /&gt;SMP: Total of 4 processors activated (6324.22 BogoMIPS).&lt;BR /&gt;print_constraints: dummy:&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;cpaddr = c0840000 wait_iram_base=c0812000&lt;BR /&gt;print_constraints: vddpu: 725 &amp;lt;--&amp;gt; 1300 mV at 700 mV fast normal&lt;BR /&gt;print_constraints: vddcore: 725 &amp;lt;--&amp;gt; 1300 mV at 1150 mV fast normal&lt;BR /&gt;print_constraints: vddsoc: 725 &amp;lt;--&amp;gt; 1300 mV at 1200 mV fast normal&lt;BR /&gt;print_constraints: vdd2p5: 2000 &amp;lt;--&amp;gt; 2775 mV at 2400 mV fast normal&lt;BR /&gt;print_constraints: vdd1p1: 800 &amp;lt;--&amp;gt; 1400 mV at 1100 mV fast normal&lt;BR /&gt;print_constraints: vdd3p0: 2800 &amp;lt;--&amp;gt; 3150 mV at 3000 mV fast normal&lt;BR /&gt;hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.&lt;BR /&gt;hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.&lt;BR /&gt;hw-breakpoint: maximum watchpoint size is 4 bytes.&lt;BR /&gt;L310 cache controller enabled&lt;BR /&gt;l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B&lt;BR /&gt;IMX usb wakeup probe&lt;BR /&gt;IMX usb wakeup probe&lt;BR /&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;BR /&gt;print_constraints: VDDA: 2500 mV&lt;BR /&gt;print_constraints: VDDIO: 3300 mV&lt;BR /&gt;machine_constraints_voltage: VDDD: unsupportable voltage constraints&lt;BR /&gt;reg-fixed-voltage reg-fixed-voltage.2: Failed to register regulator: -22&lt;BR /&gt;reg-fixed-voltage: probe of reg-fixed-voltage.2 failed with error -22&lt;BR /&gt;print_constraints: vmmc: 3300 mV&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;spi_imx imx6q-ecspi.0: probed&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;Freescale USB OTG Driver loaded, $Revision: 1.55 $&lt;BR /&gt;add wake up source irq 75&lt;BR /&gt;mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1&lt;BR /&gt;mc_pfuze 1-0008: FAB: 0 ,FIN: 0&lt;BR /&gt;print_constraints: PFUZE100_SW1A: 650 &amp;lt;--&amp;gt; 1437 mV at 1187 mV&lt;BR /&gt;print_constraints: PFUZE100_SW1B: 650 &amp;lt;--&amp;gt; 1437 mV at 650 mV&lt;BR /&gt;print_constraints: PFUZE100_SW1C: 650 &amp;lt;--&amp;gt; 1437 mV at 1187 mV&lt;BR /&gt;print_constraints: PFUZE100_SW2: 800 &amp;lt;--&amp;gt; 3950 mV at 3300 mV&lt;BR /&gt;print_constraints: PFUZE100_SW3A: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_SW3B: 400 &amp;lt;--&amp;gt; 1975 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_SW4: 400 &amp;lt;--&amp;gt; 1975 mV at 1575 mV&lt;BR /&gt;print_constraints: PFUZE100_SWBST: 5000 &amp;lt;--&amp;gt; 5150 mV at 5000 mV&lt;BR /&gt;print_constraints: PFUZE100_VSNVS: 1200 &amp;lt;--&amp;gt; 3000 mV at 1800 mV&lt;BR /&gt;print_constraints: PFUZE100_VREFDDR: at 750 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN1: 1200 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN2: 1200 &amp;lt;--&amp;gt; 1550 mV at 1500 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN3: 1800 &amp;lt;--&amp;gt; 3300 mV at 2800 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN4: 1800 &amp;lt;--&amp;gt; 3300 mV at 1800 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN5: 1800 &amp;lt;--&amp;gt; 3300 mV at 3000 mV&lt;BR /&gt;print_constraints: PFUZE100_VGEN6: 1800 &amp;lt;--&amp;gt; 3300 mV at 3300 mV&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)&lt;BR /&gt;mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed&lt;BR /&gt;mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a&lt;BR /&gt;MIPI CSI2 driver module loaded&lt;BR /&gt;Advanced Linux Sound Architecture Driver Version 1.0.24.&lt;BR /&gt;Bluetooth: Core ver 2.16&lt;BR /&gt;NET: Registered protocol family 31&lt;BR /&gt;Bluetooth: HCI device and connection manager initialized&lt;BR /&gt;Bluetooth: HCI socket layer initialized&lt;BR /&gt;Bluetooth: L2CAP socket layer initialized&lt;BR /&gt;Bluetooth: SCO socket layer initialized&lt;BR /&gt;cfg80211: Calling CRDA to update world regulatory domain&lt;BR /&gt;Switching to clocksource mxc_timer1&lt;BR /&gt;Clockevents: could not switch to one-shot mode:&lt;BR /&gt;Clockevents: could not switch to one-shot mode: dummy_timer is not functional.&lt;BR /&gt;Clockevents: could not switch to one-shot mode:&lt;BR /&gt;Could not switch to high resolution mode on CPU 2&lt;BR /&gt; dummy_timer is not functional.&lt;BR /&gt;Clockevents: could not switch to one-shot mode:&lt;BR /&gt;Could not switch to high resolution mode on CPU 0&lt;BR /&gt; dummy_timer is not functional.&lt;BR /&gt;Could not switch to high resolution mode on CPU 1&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP route cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;BR /&gt;TCP established hash table entries: 131072 (order: 8, 1048576 bytes)&lt;BR /&gt;TCP bind hash table entries: 65536 (order: 7, 786432 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 131072 bind 65536)&lt;BR /&gt;TCP reno registered&lt;BR /&gt;UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;Bus freq driver module loaded&lt;BR /&gt;Static Power Management for Freescale i.MX6&lt;BR /&gt;cpaddr = c0841000 suspend_iram_base=c08ea000&lt;BR /&gt;PM driver module loaded&lt;BR /&gt;i.MXC CPU frequency driver&lt;BR /&gt;JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;msgmni has been set to 1761&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt; dummy_timer is not functional.&lt;BR /&gt;Could not switch to high resolution mode on CPU 3&lt;BR /&gt;MIPI DSI driver module loaded&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver hdmi&lt;BR /&gt;mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1&lt;BR /&gt;fbcvt: 1920x1080@60: CVT Name - 2.073M9&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: Channel already disabled 9&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 9&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)&lt;BR /&gt;Console: switching to colour frame buffer device 240x67&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: Channel already disabled 10&lt;BR /&gt;imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 10&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb&lt;BR /&gt;_regulator_get: get() with no identifier&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: Channel already disabled 9&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 9&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: Channel already disabled 10&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 10&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver ldb&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: Channel already disabled 7&lt;BR /&gt;imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 7&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.3: ipu1-di1 already in use&lt;BR /&gt;mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16&lt;BR /&gt;imx-sdma imx-sdma: loaded firmware 1.1&lt;BR /&gt;imx-sdma imx-sdma: initialized&lt;BR /&gt;Serial: IMX driver&lt;BR /&gt;imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX&lt;BR /&gt;imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX&lt;BR /&gt;console [ttymxc0] enabled, bootconsole disabled&lt;BR /&gt;console [ttymxc0] enabled, bootconsole disabled&lt;BR /&gt;loop: module loaded&lt;BR /&gt;Can't recover from RESET HBA!&lt;BR /&gt;No sata disk.&lt;BR /&gt;m25p80 spi0.0: found m25p05-nonjedec, expected sst25vf016b&lt;BR /&gt;m25p80 spi0.0: m25p05-nonjedec (64 Kbytes)&lt;BR /&gt;Creating 2 MTD partitions on "m25p80":&lt;BR /&gt;0x000000000000-0x000000040000 : "bootloader"&lt;BR /&gt;mtd: partition "bootloader" extends beyond the end of device "m25p80" -- size truncated to 0x10000&lt;BR /&gt;0x000000010000-0x000000010000 : "kernel"&lt;BR /&gt;mtd: partition "kernel" is out of reach -- disabled&lt;BR /&gt;vcan: Virtual CAN interface driver&lt;BR /&gt;CAN device driver interface&lt;BR /&gt;flexcan netdevice driver&lt;BR /&gt;flexcan imx6q-flexcan.0: device registered (reg_base=c0938000, irq=142)&lt;BR /&gt;FEC Ethernet Driver&lt;BR /&gt;fec_enet_mii_bus: probed&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller&lt;BR /&gt;fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1&lt;BR /&gt;fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000&lt;BR /&gt;fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 1-0:1.0: USB hub found&lt;BR /&gt;hub 1-0:1.0: 1 port detected&lt;BR /&gt;add wake up source irq 72&lt;BR /&gt;fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller&lt;BR /&gt;fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2&lt;BR /&gt;fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200&lt;BR /&gt;fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00&lt;BR /&gt;hub 2-0:1.0: USB hub found&lt;BR /&gt;hub 2-0:1.0: 1 port detected&lt;BR /&gt;Initializing USB Mass Storage driver...&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;USB Mass Storage support registered.&lt;BR /&gt;ARC USBOTG Device Controller driver (1 August 2005)&lt;BR /&gt;mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;egalax_ts 1-0004: egalax_ts: failed to read firmware version&lt;BR /&gt;egalax_ts: probe of 1-0004 failed with error -5&lt;BR /&gt;egalax_ts 2-0004: egalax_ts: failed to read firmware version&lt;BR /&gt;egalax_ts: probe of 2-0004 failed with error -5&lt;BR /&gt;snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19&lt;BR /&gt;mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20&lt;BR /&gt;imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)&lt;BR /&gt;Bluetooth: Virtual HCI driver ver 1.3&lt;BR /&gt;Bluetooth: HCI UART driver ver 2.2&lt;BR /&gt;Bluetooth: HCIATH3K protocol initialized&lt;BR /&gt;Bluetooth: Generic Bluetooth USB driver ver 0.6&lt;BR /&gt;usbcore: registered new interface driver btusb&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;mmc0: Unknown controller version (3). You may experience problems.&lt;BR /&gt;mmc0: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA&lt;BR /&gt;mmc1: Unknown controller version (3). You may experience problems.&lt;BR /&gt;mmc1: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA&lt;BR /&gt;mmc2: Unknown controller version (3). You may experience problems.&lt;BR /&gt;mmc2: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA&lt;BR /&gt;VPU initialized&lt;BR /&gt;mxc_asrc registered&lt;BR /&gt;Anatop Thermal registered as thermal_zone0&lt;BR /&gt;anatop_thermal_probe: default cooling device is cpufreq!&lt;BR /&gt;usbcore: registered new interface driver usbhid&lt;BR /&gt;usbhid: USB HID core driver&lt;BR /&gt;usbcore: registered new interface driver snd-usb-audio&lt;BR /&gt;mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio&lt;BR /&gt;Cirrus Logic CS42888 ALSA SoC Codec Driver&lt;BR /&gt;i2c-core: driver [cs42888] using legacy suspend method&lt;BR /&gt;i2c-core: driver [cs42888] using legacy resume method&lt;BR /&gt;imx_3stack asoc driver&lt;BR /&gt;asoc: mxc-hdmi-soc &amp;lt;-&amp;gt; imx-hdmi-soc-dai.0 mapping ok&lt;BR /&gt;ALSA device list:&lt;BR /&gt; #0: imx-hdmi-soc&lt;BR /&gt;TCP cubic registered&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;can: controller area network core (rev 20090105 abi 8)&lt;BR /&gt;NET: Registered protocol family 29&lt;BR /&gt;can: raw protocol (rev 20090105)&lt;BR /&gt;can: broadcast manager protocol (rev 20090105 t)&lt;BR /&gt;Bluetooth: RFCOMM TTY layer initialized&lt;BR /&gt;Bluetooth: RFCOMM socket layer initialized&lt;BR /&gt;Bluetooth: RFCOMM ver 1.11&lt;BR /&gt;Bluetooth: BNEP (Ethernet Emulation) ver 1.3&lt;BR /&gt;Bluetooth: BNEP filters: protocol multicast&lt;BR /&gt;Bluetooth: HIDP (Human Interface Emulation) ver 1.2&lt;BR /&gt;lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4&lt;BR /&gt;mxc_dvfs_core_probe&lt;BR /&gt;DVFS driver module loaded&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN5: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN4: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: VDDIO: incomplete constraints, leaving on&lt;BR /&gt;regulator_init_complete: VDDA: incomplete constraints, leaving on&lt;BR /&gt;snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:05:02 UTC (302)&lt;BR /&gt;Waiting for root device /dev/mmcblk1p1...&lt;BR /&gt;mmc1: new SDHC card at address aaaa&lt;BR /&gt;mmcblk0: mmc1:aaaa SU08G 7.40 GiB&lt;BR /&gt; mmcblk0: p1&lt;BR /&gt;mmc2: new high speed DDR MMC card at address 0001&lt;BR /&gt;mmcblk1: mmc2:0001 SEM08G 7.39 GiB&lt;BR /&gt;mmcblk1boot0: mmc2:0001 SEM08G partition 1 2.00 MiB&lt;BR /&gt;mmcblk1boot1: mmc2:0001 SEM08G partition 2 2.00 MiB&lt;BR /&gt; mmcblk1: p1&lt;BR /&gt; mmcblk1boot1: unknown partition table&lt;BR /&gt; mmcblk1boot0: unknown partition table&lt;BR /&gt;EXT3-fs: barriers not enabled&lt;BR /&gt;kjournald starting. Commit interval 5 seconds&lt;BR /&gt;EXT3-fs (mmcblk1p1): using internal journal&lt;BR /&gt;EXT3-fs (mmcblk1p1): recovery complete&lt;BR /&gt;EXT3-fs (mmcblk1p1): mounted filesystem with writeback data mode&lt;BR /&gt;VFS: Mounted root (ext3 filesystem) on device 179:9.&lt;BR /&gt;Freeing init memory: 184K&lt;BR /&gt;Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.&lt;BR /&gt;[&amp;lt;80041524&amp;gt;] (unwind_backtrace+0x0/0xf8) from [&amp;lt;80481310&amp;gt;] (panic+0x74/0x18c)&lt;BR /&gt;[&amp;lt;80481310&amp;gt;] (panic+0x74/0x18c) from [&amp;lt;80481024&amp;gt;] (init_post+0xa0/0xc4)&lt;BR /&gt;[&amp;lt;80481024&amp;gt;] (init_post+0xa0/0xc4) from [&amp;lt;800089bc&amp;gt;] (kernel_init+0xfc/0x128)&lt;BR /&gt;[&amp;lt;800089bc&amp;gt;] (kernel_init+0xfc/0x128) from [&amp;lt;8003c8fc&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;BR /&gt;CPU2: stopping&lt;BR /&gt;[&amp;lt;80041524&amp;gt;] (unwind_backtrace+0x0/0xf8) from [&amp;lt;800362f8&amp;gt;] (do_IPI+0x10c/0x138)&lt;BR /&gt;[&amp;lt;800362f8&amp;gt;] (do_IPI+0x10c/0x138) from [&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4)&lt;BR /&gt;Exception stack(0xbffb5f90 to 0xbffb5fd8)&lt;BR /&gt;5f80: 00000021 80617abc bffb5fd8 00000000&lt;BR /&gt;5fa0: bffb4000 8064db04 80489408 8061adf4 1000406a 412fc09a 00000000 00000000&lt;BR /&gt;5fc0: 00000000 bffb5fd8 8003c958 8003c95c 60000013 ffffffff&lt;BR /&gt;[&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4) from [&amp;lt;8003c95c&amp;gt;] (default_idle+0x24/0x28)&lt;BR /&gt;[&amp;lt;8003c95c&amp;gt;] (default_idle+0x24/0x28) from [&amp;lt;8003cb44&amp;gt;] (cpu_idle+0xac/0xe8)&lt;BR /&gt;[&amp;lt;8003cb44&amp;gt;] (cpu_idle+0xac/0xe8) from [&amp;lt;1047e3d4&amp;gt;] (0x1047e3d4)&lt;BR /&gt;CPU3: stopping&lt;BR /&gt;[&amp;lt;80041524&amp;gt;] (unwind_backtrace+0x0/0xf8) from [&amp;lt;800362f8&amp;gt;] (do_IPI+0x10c/0x138)&lt;BR /&gt;[&amp;lt;800362f8&amp;gt;] (do_IPI+0x10c/0x138) from [&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4)&lt;BR /&gt;Exception stack(0xbff01f90 to 0xbff01fd8)&lt;BR /&gt;1f80: 00000022 80617abc bff01fd8 00000000&lt;BR /&gt;1fa0: bff00000 8064db04 80489408 8061adf4 1000406a 412fc09a 00000000 00000000&lt;BR /&gt;1fc0: 00000000 bff01fd8 8003c958 8003c95c 60000013 ffffffff&lt;BR /&gt;[&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4) from [&amp;lt;8003c95c&amp;gt;] (default_idle+0x24/0x28)&lt;BR /&gt;[&amp;lt;8003c95c&amp;gt;] (default_idle+0x24/0x28) from [&amp;lt;8003cb44&amp;gt;] (cpu_idle+0xac/0xe8)&lt;BR /&gt;[&amp;lt;8003cb44&amp;gt;] (cpu_idle+0xac/0xe8) from [&amp;lt;1047e3d4&amp;gt;] (0x1047e3d4)&lt;BR /&gt;CPU1: stopping&lt;BR /&gt;[&amp;lt;80041524&amp;gt;] (unwind_backtrace+0x0/0xf8) from [&amp;lt;800362f8&amp;gt;] (do_IPI+0x10c/0x138)&lt;BR /&gt;[&amp;lt;800362f8&amp;gt;] (do_IPI+0x10c/0x138) from [&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4)&lt;BR /&gt;Exception stack(0xbfd29de0 to 0xbfd29e28)&lt;BR /&gt;9de0: 00000000 0000000a 00000001 00000001 00000282 bfd28000 80034c00 bfd28000&lt;BR /&gt;9e00: 80608040 806534a0 0bfdc000 00000001 00000000 bfd29e28 80068dcc 80068840&lt;BR /&gt;9e20: 20000113 ffffffff&lt;BR /&gt;[&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4) from [&amp;lt;80068840&amp;gt;] (__do_softirq+0x50/0x154)&lt;BR /&gt;[&amp;lt;80068840&amp;gt;] (__do_softirq+0x50/0x154) from [&amp;lt;80068dcc&amp;gt;] (irq_exit+0x94/0x9c)&lt;BR /&gt;[&amp;lt;80068dcc&amp;gt;] (irq_exit+0x94/0x9c) from [&amp;lt;800362cc&amp;gt;] (do_IPI+0xe0/0x138)&lt;BR /&gt;[&amp;lt;800362cc&amp;gt;] (do_IPI+0xe0/0x138) from [&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4)&lt;BR /&gt;Exception stack(0xbfd29e88 to 0xbfd29ed0)&lt;BR /&gt;9e80: 8064f060 60000093 80627c7c 80627c7c 8064f06a 8064f099&lt;BR /&gt;9ea0: 80627c1c 8064efa8 00000035 8064f06a 00000003 00000001 60000013 bfd29ed0&lt;BR /&gt;9ec0: 80064260 800643ac 60000013 ffffffff&lt;BR /&gt;[&amp;lt;8003b94c&amp;gt;] (__irq_svc+0x4c/0xc4) from [&amp;lt;800643ac&amp;gt;] (vprintk+0x38c/0x50c)&lt;BR /&gt;[&amp;lt;800643ac&amp;gt;] (vprintk+0x38c/0x50c) from [&amp;lt;80481448&amp;gt;] (printk+0x20/0x30)&lt;BR /&gt;[&amp;lt;80481448&amp;gt;] (printk+0x20/0x30) from [&amp;lt;8017e72c&amp;gt;] (kjournald+0x88/0x214)&lt;BR /&gt;[&amp;lt;8017e72c&amp;gt;] (kjournald+0x88/0x214) from [&amp;lt;8007cb28&amp;gt;] (kthread+0x80/0x88)&lt;BR /&gt;[&amp;lt;8007cb28&amp;gt;] (kthread+0x80/0x88) from [&amp;lt;8003c8fc&amp;gt;] (kernel_thread_exit+0x0/0x8)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 05:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SABRE-Board-for-Smart-Devices-Linux-Boot-Fail-Kernel-panic/m-p/552704#M86309</guid>
      <dc:creator>mianbohuang</dc:creator>
      <dc:date>2016-08-24T05:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 SABRE Board for Smart Devices Linux Boot Fail Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SABRE-Board-for-Smart-Devices-Linux-Boot-Fail-Kernel-panic/m-p/552705#M86310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mianbo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to prepare card using attached Linux Guide&lt;/P&gt;&lt;P&gt;Chapter 8 Using a Linux Host to Set Up an SD/MMC Card&lt;/P&gt;&lt;P&gt;and check procedure using Demo Images&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product" title="http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=L3.0.101_4.1.1_IM6QDLS_BUNDLE&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=133…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 00:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-SABRE-Board-for-Smart-Devices-Linux-Boot-Fail-Kernel-panic/m-p/552705#M86310</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-25T00:04:43Z</dc:date>
    </item>
  </channel>
</rss>