<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックNitrogen6_max uboot from eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-max-uboot-from-eMMC/m-p/552548#M86291</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are attempting to boot nitrogen6_max board from the eMMC.&lt;/P&gt;&lt;P&gt;It seems we'll have to program certain eFUSE since there is no boot-switch option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since these changes are irreversible, I wanted to know if it was safe to program the following fuses with following values? Are these changes sufficient to enable eMMC boot on nitrogen6_max board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before&lt;/P&gt;&lt;P&gt;BOOT_CFG[4:0]: 0x00000005: = 0x18000030&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After&lt;/P&gt;&lt;P&gt;BOOT_CFG[4:0]: 0x00000005: = 0x18005878&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Anand Mistry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jul 2016 14:33:11 GMT</pubDate>
    <dc:creator>anandmistryk</dc:creator>
    <dc:date>2016-07-08T14:33:11Z</dc:date>
    <item>
      <title>Nitrogen6_max uboot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-max-uboot-from-eMMC/m-p/552548#M86291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are attempting to boot nitrogen6_max board from the eMMC.&lt;/P&gt;&lt;P&gt;It seems we'll have to program certain eFUSE since there is no boot-switch option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since these changes are irreversible, I wanted to know if it was safe to program the following fuses with following values? Are these changes sufficient to enable eMMC boot on nitrogen6_max board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before&lt;/P&gt;&lt;P&gt;BOOT_CFG[4:0]: 0x00000005: = 0x18000030&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After&lt;/P&gt;&lt;P&gt;BOOT_CFG[4:0]: 0x00000005: = 0x18005878&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Anand Mistry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jul 2016 14:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-max-uboot-from-eMMC/m-p/552548#M86291</guid>
      <dc:creator>anandmistryk</dc:creator>
      <dc:date>2016-07-08T14:33:11Z</dc:date>
    </item>
  </channel>
</rss>