<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6UL resolution under VGA in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549226#M86037</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The default screen that comes with the board is 480x272. Here is a&amp;nbsp;link to a video we did of the UL running our demos at 480x272&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cranksoftware.com/demo_image/imx6ultralite" title="http://cranksoftware.com/demo_image/imx6ultralite"&gt;iMX6UltraLite | Crank Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Aug 2016 17:49:10 GMT</pubDate>
    <dc:creator>CrankSoftware</dc:creator>
    <dc:date>2016-08-23T17:49:10Z</dc:date>
    <item>
      <title>iMX6UL resolution under VGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549225#M86036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm find misleading table at the attached pdf file's 25 page.&lt;/P&gt;&lt;P&gt;The table at the right side describes the iMX6UL processor's supported resolutions. &lt;BR /&gt;As I see there are no display support under VGA resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My intuition is that lower resolutions ! have to OK for the UltraLite, but I have to be sure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the UltraLite with a 480x272 resolution display is it possible ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards János&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Aug 2016 13:35:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549225#M86036</guid>
      <dc:creator>julbert</dc:creator>
      <dc:date>2016-08-23T13:35:39Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6UL resolution under VGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549226#M86037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The default screen that comes with the board is 480x272. Here is a&amp;nbsp;link to a video we did of the UL running our demos at 480x272&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cranksoftware.com/demo_image/imx6ultralite" title="http://cranksoftware.com/demo_image/imx6ultralite"&gt;iMX6UltraLite | Crank Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Aug 2016 17:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549226#M86037</guid>
      <dc:creator>CrankSoftware</dc:creator>
      <dc:date>2016-08-23T17:49:10Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6UL resolution under VGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549227#M86038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi János&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, lower resolutions are supported by UltraLite too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 00:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549227#M86038</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-24T00:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6UL resolution under VGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549228#M86039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Jason,&lt;BR /&gt;&lt;BR /&gt;Thanks for the fast reply! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 07:13:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6UL-resolution-under-VGA/m-p/549228#M86039</guid>
      <dc:creator>julbert</dc:creator>
      <dc:date>2016-08-24T07:13:13Z</dc:date>
    </item>
  </channel>
</rss>