<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: uboot nand read error after update to 4.1 kernel ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uboot-nand-read-error-after-update-to-4-1-kernel/m-p/548501#M85982</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try attached kobs-ng patch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Aug 2016 07:19:31 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-08-23T07:19:31Z</dc:date>
    <item>
      <title>uboot nand read error after update to 4.1 kernel ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-nand-read-error-after-update-to-4-1-kernel/m-p/548500#M85981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Am able to boot from nand just fine with 3.14 kernel but after updating to the&lt;/P&gt;&lt;P&gt;4.1 kernel I now get the following uboot error when uboot tries to read the&lt;/P&gt;&lt;P&gt;kernel from NAND:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; NAND read: device 0 offset 0x4000000, size 0x800000&lt;/P&gt;&lt;P&gt;&amp;nbsp; NAND read from offset 5000000 failed -74&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems to be a problem with nandwrite and the newer kernel. If I write&lt;/P&gt;&lt;P&gt;the kernel with nandwrite under the 3.14 kernel it works ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using kobs-ng 5.4 and nandwrite from the imx_4.1.15_1.0.0_ga yocto build.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 13:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-nand-read-error-after-update-to-4-1-kernel/m-p/548500#M85981</guid>
      <dc:creator>SJA</dc:creator>
      <dc:date>2016-08-22T13:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: uboot nand read error after update to 4.1 kernel ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-nand-read-error-after-update-to-4-1-kernel/m-p/548501#M85982</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try attached kobs-ng patch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Aug 2016 07:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-nand-read-error-after-update-to-4-1-kernel/m-p/548501#M85982</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-08-23T07:19:31Z</dc:date>
    </item>
  </channel>
</rss>