<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: About charged using LICELL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-charged-using-LICELL/m-p/548325#M85960</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, igor&lt;/P&gt;&lt;P&gt;Thank you for answering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the OFF mode, it was understood that the charge is stopped.&lt;/P&gt;&lt;P&gt;2 might cause for coin battery not fully charged.&lt;/P&gt;&lt;P&gt;Try a little more experimental.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-satoshi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jun 2016 02:31:24 GMT</pubDate>
    <dc:creator>okamotosatoshi</dc:creator>
    <dc:date>2016-06-21T02:31:24Z</dc:date>
    <item>
      <title>About charged using LICELL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-charged-using-LICELL/m-p/548323#M85958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is charging of the coin battery in MMPF0200.&lt;/P&gt;&lt;P&gt;VIN is supplied always 4.2V.&lt;/P&gt;&lt;P&gt;Coin Cell (LICELL) is connected to the coin battery "ML-621S / DN".&lt;/P&gt;&lt;P&gt;(Coin Cell is about 2.1V)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Document Number: MMPF0200　Rev. 6.0, 3/2015&lt;/P&gt;&lt;P&gt;　P77 VSNVS LDO/Switch&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, we want information about the following two points.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;①During OFF mode, Can continue to charge the coin battery?&lt;/P&gt;&lt;P&gt;　After the transition to the OFF mode, the voltage of the coin battery will decrease.&lt;/P&gt;&lt;P&gt;②During the OFF mode, even if VIN is always input will be discharged from the coin battery.&lt;/P&gt;&lt;P&gt;　Selection of the VIN and Coin Cell will switching to physical? (using "Input Sense/Selector")&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following state has been confirmed.&lt;/P&gt;&lt;P&gt;When cutting the Coin the Cell, voltage of the coin battery is not reduced.&lt;/P&gt;&lt;P&gt;When cutting the VSNVS, voltage of the coin battery is not reduced.&lt;/P&gt;&lt;P&gt;If the Coin Cell and VSNVS is connected, the voltage drop of the coin battery is made early.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-satoshi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 08:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-charged-using-LICELL/m-p/548323#M85958</guid>
      <dc:creator>okamotosatoshi</dc:creator>
      <dc:date>2016-06-20T08:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: About charged using LICELL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-charged-using-LICELL/m-p/548324#M85959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the OFF state, coin cell charging is not available&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59925iF226130C06B88F13/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 00:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-charged-using-LICELL/m-p/548324#M85959</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-21T00:24:14Z</dc:date>
    </item>
    <item>
      <title>Re: About charged using LICELL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-charged-using-LICELL/m-p/548325#M85960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, igor&lt;/P&gt;&lt;P&gt;Thank you for answering.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the OFF mode, it was understood that the charge is stopped.&lt;/P&gt;&lt;P&gt;2 might cause for coin battery not fully charged.&lt;/P&gt;&lt;P&gt;Try a little more experimental.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-satoshi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 02:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-charged-using-LICELL/m-p/548325#M85960</guid>
      <dc:creator>okamotosatoshi</dc:creator>
      <dc:date>2016-06-21T02:31:24Z</dc:date>
    </item>
  </channel>
</rss>