<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIPI DSI commands length in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-commands-length/m-p/547454#M85890</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to MIPI DSI Specification, Generic Short Write with 1 Parameter should be 3 bytes long: DI (0x13) + one parameter + ECC. IMX6 always sends at least 4 bytes, in this case: DI + one parameter + one byte of payload data + ECC. Why is so? &lt;/P&gt;&lt;P&gt;Is there any way to send only 2 or 3 bytes?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2016 08:14:10 GMT</pubDate>
    <dc:creator>jotes</dc:creator>
    <dc:date>2016-07-28T08:14:10Z</dc:date>
    <item>
      <title>MIPI DSI commands length</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-commands-length/m-p/547454#M85890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to MIPI DSI Specification, Generic Short Write with 1 Parameter should be 3 bytes long: DI (0x13) + one parameter + ECC. IMX6 always sends at least 4 bytes, in this case: DI + one parameter + one byte of payload data + ECC. Why is so? &lt;/P&gt;&lt;P&gt;Is there any way to send only 2 or 3 bytes?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 08:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-commands-length/m-p/547454#M85890</guid>
      <dc:creator>jotes</dc:creator>
      <dc:date>2016-07-28T08:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI DSI commands length</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-commands-length/m-p/547455#M85891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MIPI DSI Host controller module supports short write packets type. The issue you observe most likely depends on the driver implementation.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2016 10:24:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-commands-length/m-p/547455#M85891</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-07-29T10:24:17Z</dc:date>
    </item>
  </channel>
</rss>