<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックTCP/IP on i.MX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/TCP-IP-on-i-MX6/m-p/547452#M85888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to create a small TCP/IP server on QT (my system is based on i.MX6 and Yocto).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you give me some examples ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UPDATE: I used the following example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.bogotobogo.com/Qt/Qt5_QTcpServer_Client_Server.php" title="http://www.bogotobogo.com/Qt/Qt5_QTcpServer_Client_Server.php"&gt;http://www.bogotobogo.com/Qt/Qt5_QTcpServer_Client_Server.php&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I created a simple Client on Windows with C# to test the Communication and all is working fine ! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Jun 2016 10:32:15 GMT</pubDate>
    <dc:creator>simonetolotti</dc:creator>
    <dc:date>2016-06-20T10:32:15Z</dc:date>
    <item>
      <title>TCP/IP on i.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TCP-IP-on-i-MX6/m-p/547452#M85888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to create a small TCP/IP server on QT (my system is based on i.MX6 and Yocto).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you give me some examples ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UPDATE: I used the following example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.bogotobogo.com/Qt/Qt5_QTcpServer_Client_Server.php" title="http://www.bogotobogo.com/Qt/Qt5_QTcpServer_Client_Server.php"&gt;http://www.bogotobogo.com/Qt/Qt5_QTcpServer_Client_Server.php&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I created a simple Client on Windows with C# to test the Communication and all is working fine ! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 10:32:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TCP-IP-on-i-MX6/m-p/547452#M85888</guid>
      <dc:creator>simonetolotti</dc:creator>
      <dc:date>2016-06-20T10:32:15Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP on i.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/TCP-IP-on-i-MX6/m-p/547453#M85889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can add the server you need (httpd for example) into Yocto configuration to build the service.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 11:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/TCP-IP-on-i-MX6/m-p/547453#M85889</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-06-21T11:03:31Z</dc:date>
    </item>
  </channel>
</rss>