<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Bitbake options in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545734#M85788</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to run core-image-minimal and it is running 3.14.28 version&amp;nbsp; instead if 3.14.38...the 3.14.28 does not support for 3.14.38&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jul 2016 05:23:39 GMT</pubDate>
    <dc:creator>chandraevolute</dc:creator>
    <dc:date>2016-07-08T05:23:39Z</dc:date>
    <item>
      <title>Bitbake options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545730#M85784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;what is the difference between bitbake -c compile -f linu-imx and bitbake linu-imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;whenI run bitbake -c compile -f linu-imx this command it executed succesfully but when I try to do bitbake linu-imx it fails&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 07:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545730#M85784</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2016-07-07T07:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545731#M85785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please look at the following&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94953"&gt;Useful bitbake commands&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 07:17:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545731#M85785</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-07-07T07:17:36Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545732#M85786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/YuriMuhin_ng"&gt;YuriMuhin_ng&lt;/A&gt; got the difference...&lt;/P&gt;&lt;P&gt;one more issue is when I do bitbake fsl-image-gui the .sdcard image is showing 880MB size. How can I reduce the rootfs. where as my zImage is 4MB only.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 07:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545732#M85786</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2016-07-07T07:24:51Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545733#M85787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; the .sdcard image includes U-boot, kernel and file system.&lt;/P&gt;&lt;P&gt; It&amp;nbsp; requires to remove non-needed packages in order to reduce file system.&lt;/P&gt;&lt;P&gt;Perhaps it would be better to use core-image-minimal configuration. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 09:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545733#M85787</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-07-07T09:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545734#M85788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to run core-image-minimal and it is running 3.14.28 version&amp;nbsp; instead if 3.14.38...the 3.14.28 does not support for 3.14.38&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jul 2016 05:23:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-options/m-p/545734#M85788</guid>
      <dc:creator>chandraevolute</dc:creator>
      <dc:date>2016-07-08T05:23:39Z</dc:date>
    </item>
  </channel>
</rss>