<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CRC value in CAN Loopback testing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CRC-value-in-CAN-Loopback-testing/m-p/542903#M85533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am testing "Can" interface using "canutils" utility. Currently i am testing a can interface with "loopback" mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i am capturing packets sent through cansend utility using tcpdump i can not see CRC field filled in packets i.e. its value is 0. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also when i check "flexcan.c" file, i cannot find any code for filling CRC value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone please help why no CRC value is filled?&lt;/P&gt;&lt;P&gt;Is it because of "loopback" mode?&lt;/P&gt;&lt;P&gt;At which point exaclty the "crc" field on CAN frame is filled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Khushboo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jul 2016 14:15:00 GMT</pubDate>
    <dc:creator>khushboosharma</dc:creator>
    <dc:date>2016-07-27T14:15:00Z</dc:date>
    <item>
      <title>CRC value in CAN Loopback testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CRC-value-in-CAN-Loopback-testing/m-p/542903#M85533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am testing "Can" interface using "canutils" utility. Currently i am testing a can interface with "loopback" mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i am capturing packets sent through cansend utility using tcpdump i can not see CRC field filled in packets i.e. its value is 0. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also when i check "flexcan.c" file, i cannot find any code for filling CRC value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone please help why no CRC value is filled?&lt;/P&gt;&lt;P&gt;Is it because of "loopback" mode?&lt;/P&gt;&lt;P&gt;At which point exaclty the "crc" field on CAN frame is filled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Khushboo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 14:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CRC-value-in-CAN-Loopback-testing/m-p/542903#M85533</guid>
      <dc:creator>khushboosharma</dc:creator>
      <dc:date>2016-07-27T14:15:00Z</dc:date>
    </item>
    <item>
      <title>Re: CRC value in CAN Loopback testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CRC-value-in-CAN-Loopback-testing/m-p/542904#M85534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Khushboo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for crc usage one can look at sect.26.6.9.5 Arbitration and Matching Timing&lt;/P&gt;&lt;P&gt;i.MX6DQ Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX6DQRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/323257"&gt;Linux driver for i.mx6 flexcan mailbox&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 23:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CRC-value-in-CAN-Loopback-testing/m-p/542904#M85534</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-27T23:55:05Z</dc:date>
    </item>
  </channel>
</rss>