<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: yocto build fail</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/yocto-build-fail/m-p/542652#M85499</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;thanks for you help , i have rebuild the project. &lt;/P&gt;&lt;P&gt;but i got another problem：&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/431579"&gt;bitbake u-boot-imx fail&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 Jul 2016 06:30:50 GMT</pubDate>
    <dc:creator>半醒的狐狸</dc:creator>
    <dc:date>2016-07-30T06:30:50Z</dc:date>
    <item>
      <title>yocto build fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-build-fail/m-p/542650#M85497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; i have created a yocto project，and&amp;nbsp; bitbake core-image-sato， it failed。&lt;BR /&gt;the log ：&lt;/P&gt;&lt;P&gt;ERROR: core-image-sato-1.0-r0 do_rootfs: &lt;BR /&gt;ERROR: ld.so: object '/lib/$LIB/liblsp.so' from /etc/ld.so.preload cannot be preloaded (wrong ELF class: ELFCLASS64): ignored.&lt;BR /&gt;NOTE: &amp;gt; Executing update_pixbuf_cache intercept ...&lt;BR /&gt;ERROR: ld.so: object '/lib/$LIB/liblsp.so' from /etc/ld.so.preload cannot be preloaded (wrong ELF class: ELFCLASS64): ignored.&lt;BR /&gt;NOTE: &amp;gt; Executing update_font_cache intercept ...&lt;BR /&gt;ERROR: ld.so: object '/lib/$LIB/liblsp.so' from /etc/ld.so.preload cannot be preloaded (wrong ELF class: ELFCLASS64): ignored.&lt;BR /&gt;FC_DEBUG=1&lt;BR /&gt;[/home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/rootfs]/usr/share/fonts: skipping, existing cache is valid: 0 fonts, 1 dirs&lt;BR /&gt;[/home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/rootfs]/usr/share/fonts/ttf: skipping, existing cache is valid: 12 fonts, 0 dirs&lt;BR /&gt;Re-scanning [/home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/rootfs]/usr/share/fonts: caching, new cache contents: 0 fonts, 1 dirs&lt;/P&gt;&lt;P&gt;ERROR: core-image-sato-1.0-r0 do_rootfs: Function failed: do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/temp/log.do_rootfs.6559&lt;BR /&gt;ERROR: Task 9 (/home/lyi/imx/fsl-community-bsp/sources/poky/meta/recipes-sato/images/core-image-sato.bb, do_rootfs) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what's the mean of this error，and hwo to solve ？&lt;/P&gt;&lt;P&gt;thanks for you help!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 02:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-build-fail/m-p/542650#M85497</guid>
      <dc:creator>半醒的狐狸</dc:creator>
      <dc:date>2016-07-27T02:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: yocto build fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-build-fail/m-p/542651#M85498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide more information on what BSP you are using and for which MACHINE? If you could share your local.conf file the required information should be in there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the information you provide I’m assuming you are using the Community BSP although you do not specify which branch. Branches Jethro and Krogoth do support the i.MX6UL EVK but earlier branches may not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 13:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-build-fail/m-p/542651#M85498</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-07-28T13:53:01Z</dc:date>
    </item>
    <item>
      <title>Re: yocto build fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-build-fail/m-p/542652#M85499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;thanks for you help , i have rebuild the project. &lt;/P&gt;&lt;P&gt;but i got another problem：&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/431579"&gt;bitbake u-boot-imx fail&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Jul 2016 06:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-build-fail/m-p/542652#M85499</guid>
      <dc:creator>半醒的狐狸</dc:creator>
      <dc:date>2016-07-30T06:30:50Z</dc:date>
    </item>
  </channel>
</rss>